EtherNet/IP™ Adapter  1.03.02
User Reference Manual

◆ EI_API_ADP_setSerialNumber()

uint32_t EI_API_ADP_setSerialNumber ( T *  pAdp_p,
uint32_t  serialNumber_p 
)

Set the adapter's unique serial number (Instance Attribute ID: 6).

Function to set a unique serial number of the adapter selected by parameter pAdp_p. This attribute is used in conjunction with the vendor ID to form a unique identifier for each device on any CIP network. It is in the responsibility of the device vendor to guarantee that the serial number is unique across all of the vendor's devices.

The value zero is not a valid serial number and shall not be assigned to a product.

Parameters
[in]pAdp_pPointer to the adapter.
[in]serialNumber_pNew serial number.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
// Set serial number to 101
errCode = EI_API_ADP_setSerialNumber(pEI_API_ADP, 0x065);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:202
ETHIP_API uint32_t EI_API_ADP_setSerialNumber(T *pAdp_p, uint32_t serialNumber_p)
Set the adapter's unique serial number (Instance Attribute ID: 6).
Definition: EI_API_ADP_main.c:1501
See also
EI_API_ADP_getSerialNumber EI_API_ADP_EError_t