#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
ei_api_adp_error_t errCode;
uint8_t numInterfaces = 1;
for (int i = 0; i < 2; i++)
{
}
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:202
ETHIP_API uint32_t EI_API_ADP_setIntfConfig(T *adp, uint8_t intfId, EI_API_ADP_UIntfConf_t intfConfig)
Set the adapter Ethernet interface configuration (Instance Attribute ID: 6).
Definition: EI_API_ADP_main.c:3658
uint8_t all
Access all bits.
Definition: EI_API_def.h:125
Struct to use as function parameters (attribute parameters)
Definition: EI_API_def.h:124