void EC_API_SLV_EEPROM_cbRegisterLoad | ( | EC_API_SLV_SHandle_t * | pEcSlaveApi_p, |
void * | pContext_p, | ||
EC_API_SLV_CBEepromLoad_t | cbFunc_p | ||
) |
Register a function lo load the eeprom content.
If the EEPROM content is stored permanently, then the DTK Stack requires a function to access the content. If nothing is defined, then the EEPROM content is generated dynamically based on the application parameters.
[in] | pEcSlaveApi_p | Slave API Handle Instance |
[in] | pContext_p | Load EEPROM Callback context |
[in] | cbFunc_p | Load EEPROM Callback |