uint32_t EC_API_SLV_PDO_enabled | ( | EC_API_SLV_SHandle_t * | pEcSlaveApi_p, |
EC_API_SLV_SPdo_t * | pPdo_p, | ||
bool * | pEnabled_p | ||
) |
Return if the PDO is assigned to the syncManager.
[in] | pEcSlaveApi_p | pointer to API instance. |
[in] | pPdo_p | pointer to PDO. |
[out] | pEnabled_p | PDO is assigned to SyncManager or not. |