uint32_t EC_API_SLV_EoE_sendFrame | ( | EC_API_SLV_SHandle_t * | pEcSlaveApi_p, |
uint16_t | length_p, | ||
uint8_t * | pData_p | ||
) |
This is the function to send EoE frames.
Use this function to send Ethernet frames over the EtherCAT network
[in] | pEcSlaveApi_p | The pointer to the EtherCAT API instance. |
[in] | length_p | The data length |
[in] | pData_p | The pointer to the data |