uint32_t EC_API_SLV_setStandardMailbox | ( | EC_API_SLV_SHandle_t * | pEcSlaveApi_p, |
uint16_t | rxOffset_p, | ||
uint16_t | rxSize_p, | ||
uint16_t | txOffset_p, | ||
uint16_t | txSize_p | ||
) |
Set Standard Mailbox Configuration.
[in] | pEcSlaveApi_p | The pointer to the EtherCAT API instance. |
[in] | rxOffset_p | Start offset of bootstrap Receive Mailbox. |
[in] | rxSize_p | Size of bootstrap Receive Mailbox. |
[in] | txOffset_p | Start offset of bootstrap Send Mailbox. |
[in] | txSize_p | Size of bootstrap Send Mailbox. |