EtherCAT Slave  1.04.03

◆ EC_API_SLV_setErrorRegister()

uint32_t EC_API_SLV_setErrorRegister ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
EC_API_SLV_EErrorRegister_t  errorRegister_p 
)

Error register value defined in ETG1000.6 Error Register Table.

Set Error register value, used by Object 0x1001 in Object Dictionary.

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
[in]errorRegister_pNew Error Register Value.
Returns
ErrorCode DTK Error code.
Example
#include <ecSlvApi.h>
// the Call
EC_API_SLV_eERR_TEMPERATURE_ERROR
@ EC_API_SLV_eERR_TEMPERATURE_ERROR
Temperature error.
Definition: ecSlvApi.h:114
EC_API_SLV_setErrorRegister
uint32_t EC_API_SLV_setErrorRegister(EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_EErrorRegister_t errorRegister_p)
Error register value defined in ETG1000.6 Error Register Table.
Definition: ecSlvApiStub.c:1477