EtherCAT Slave  1.04.03

◆ EC_API_SLV_reset()

uint32_t EC_API_SLV_reset ( EC_API_SLV_SHandle_t pEcSlaveApi_p)

Reset configuration to default values.

Reset Pdo Assignments, mappings and any configuration to default values

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
Returns
EC_API_EError_t Returns the API error code.
Example
#include <ecSlvApi.h>
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
uint32t retVal = 0;
// the Call
retVal = EC_API_SLV_reset(S_ecSlvApiHdl);
EC_API_SLV_SHandle_t
struct EC_API_SLV_SHandle EC_API_SLV_SHandle_t
EC_API_SLV_SHandle_t describes the EtherCAT Slave API.
Definition: ecSlvApi.h:134
EC_API_SLV_reset
uint32_t EC_API_SLV_reset(EC_API_SLV_SHandle_t *pEcSlaveApi_p)
Reset configuration to default values.
Definition: ecSlvApiStub.c:815