This module contains APIs to program and use the UART.
Files | |
file | uart/v0/uart.h |
This file contains the prototype of UART driver APIs. | |
Data Structures | |
struct | UART_Transaction |
Data structure used with UART_read() and UART_write() More... | |
struct | UART_Params |
UART Parameters. More... | |
struct | UART_Attrs |
UART instance attributes - used during init time. More... | |
struct | UART_Object |
UART driver object. More... | |
struct | UART_Config |
UART global configuration array. More... | |
Functions | |
void | UART_init (void) |
This function initializes the UART module. More... | |
void | UART_deinit (void) |
This function de-initializes the UART module. More... | |
UART_Handle | UART_open (uint32_t index, const UART_Params *prms) |
This function opens a given UART peripheral. More... | |
void | UART_close (UART_Handle handle) |
Function to close a UART peripheral specified by the UART handle. More... | |
int32_t | UART_write (UART_Handle handle, UART_Transaction *trans) |
Function to perform UART write operation. More... | |
int32_t | UART_read (UART_Handle handle, UART_Transaction *trans) |
Function to perform UART read operation. More... | |
int32_t | UART_writeCancel (UART_Handle handle, UART_Transaction *trans) |
Function to perform UART canceling of current write transaction. More... | |
int32_t | UART_readCancel (UART_Handle handle, UART_Transaction *trans) |
Function to perform UART canceling of current read transaction. More... | |
UART_Handle | UART_getHandle (uint32_t index) |
Function to return a open'ed UART handle given a UART instance index. More... | |
void | UART_flushTxFifo (UART_Handle handle) |
Function to flush a TX FIFO of peripheral specified by the UART handle. More... | |
static void | UART_Params_init (UART_Params *prms) |
Function to initialize the UART_Params struct to its defaults. More... | |
static void | UART_Transaction_init (UART_Transaction *trans) |
Function to initialize the UART_Transaction struct to its defaults. More... | |
uint32_t | UART_getBaseAddr (UART_Handle handle) |
Function to get base address of UART instance of a particular handle. More... | |
void | UART_enableLoopbackMode (uint32_t baseAddr) |
Function to enable loopback mode. This function is for internal use. Not recommended for customers to use. More... | |
void | UART_disableLoopbackMode (uint32_t baseAddr) |
Function to disable loopback mode. This function is for internal use. Not recommended for customers to use. More... | |
static void | UART_putChar (uint32_t baseAddr, uint8_t byteTx) |
This API writes a byte to the Transmitter FIFO without checking for the emptiness of the Transmitter FIFO or the Transmitter Shift Register(TSR). More... | |
static uint32_t | UART_getChar (uint32_t baseAddr, uint8_t *pChar) |
This API reads a byte from the Receiver Buffer Register (RBR). It checks once if any character is ready to be read. More... | |
static void | UART_intrEnable (uint32_t baseAddr, uint32_t intrFlag) |
This API enables the specified interrupts in the UART mode of operation. More... | |
static void | UART_intrDisable (uint32_t baseAddr, uint32_t intrFlag) |
This API disables the specified interrupts in the UART mode of operation. More... | |
static void | UART_intr2Enable (uint32_t baseAddr, uint32_t intrFlag) |
This API enables the specified interrupts in the UART mode of operation for IER2. More... | |
static void | UART_intr2Disable (uint32_t baseAddr, uint32_t intrFlag) |
This API disables the specified interrupts in the UART mode of operation for IER2. More... | |
static uint32_t | UART_getIntrIdentityStatus (uint32_t baseAddr) |
This API determines the UART Interrupt Status. More... | |
static uint32_t | UART_getIntr2Status (uint32_t baseAddr) |
This API determines the UART Interrupt Status 2. More... | |
static uint32_t | UART_checkCharsAvailInFifo (uint32_t baseAddr) |
This API checks if the RX FIFO (or RHR in non-FIFO mode) has atleast one byte of data to be read. More... | |
static uint32_t | UART_readLineStatus (uint32_t baseAddr) |
This API reads the line status register value. More... | |
static uint8_t | UART_getCharFifo (uint32_t baseAddr, uint8_t *readBuf) |
This API reads the data present at the top of the RX FIFO, that is, the data in the Receive Holding Register(RHR). However before reading the data from RHR, it checks for RX error. More... | |
Typedefs | |
typedef void * | UART_Handle |
A handle that is returned from a UART_open() call. More... | |
typedef void(* | UART_CallbackFxn) (UART_Handle handle, UART_Transaction *transaction) |
The definition of a callback function used by the UART driver when used in UART_TRANSFER_MODE_CALLBACK. More... | |
Macros | |
#define | UART_FIFO_SIZE (64U) |
Uart FIFO Size. More... | |
#define | UART_TRANSMITEMPTY_TRIALCOUNT (3000U) |
Timeout in ms used for TX FIFO empty at the time of delete. Three seconds is more than sufficient to transfer 64 bytes (FIFO size) at the lowest baud rate of 2400. More... | |
#define | UART_ERROR_COUNT (0x00FFFFFFU) |
Count Value to check error in the recieved byte More... | |
Transfer Status Code | |
Status codes that are set by the UART driver | |
#define | UART_TRANSFER_STATUS_SUCCESS (0U) |
Transaction success. More... | |
#define | UART_TRANSFER_STATUS_TIMEOUT (1U) |
Time out error. More... | |
#define | UART_TRANSFER_STATUS_ERROR_BI (2U) |
Break condition error. More... | |
#define | UART_TRANSFER_STATUS_ERROR_FE (3U) |
Framing error. More... | |
#define | UART_TRANSFER_STATUS_ERROR_PE (4U) |
Parity error. More... | |
#define | UART_TRANSFER_STATUS_ERROR_OE (5U) |
Overrun error. More... | |
#define | UART_TRANSFER_STATUS_CANCELLED (6U) |
Cancelled. More... | |
#define | UART_TRANSFER_STATUS_STARTED (7U) |
Transaction started. More... | |
#define | UART_TRANSFER_STATUS_READ_TIMEOUT (8U) |
Read timeout error. More... | |
#define | UART_TRANSFER_STATUS_ERROR_INUSE (9U) |
UART is currently in use. More... | |
#define | UART_TRANSFER_STATUS_ERROR_OTH (10U) |
Other errors. More... | |
Transfer Mode | |
This determines whether the driver operates synchronously or asynchronously In UART_TRANSFER_MODE_BLOCKING mode UART_read() and UART_write() blocks code execution until the transaction has completed In UART_TRANSFER_MODE_CALLBACK UART_read() and UART_write() does not block code execution and instead calls a UART_CallbackFxn callback function when the transaction has completed | |
#define | UART_TRANSFER_MODE_BLOCKING (0U) |
UART read/write APIs blocks execution. This mode can only be used when called within a Task context. More... | |
#define | UART_TRANSFER_MODE_CALLBACK (1U) |
UART read/write APIs does not block code execution and will call a UART_CallbackFxn. This mode can be used in a Task, Swi, or Hwi context. More... | |
UART Read length | |
This enumeration defines the return modes for UART_read(). UART_READ_RETURN_MODE_FULL unblocks or performs a callback when the read buffer has been filled with the number of bytes passed to UART_read(). UART_READ_RETURN_MODE_PARTIAL unblocks or performs a callback whenever a read timeout error occurs on the UART peripheral. The read timeout occurs if the read FIFO is non-empty and no new data has been received for a specific device/baudrate dependent number of clock cycles. This mode can be used when the exact number of bytes to be read is not known. | |
#define | UART_READ_RETURN_MODE_FULL (0U) |
Unblock/callback when buffer is full. More... | |
#define | UART_READ_RETURN_MODE_PARTIAL (1U) |
Unblock/callback when no new data comes in. More... | |
UART data length | |
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
#define | UART_LEN_5 (0U) |
#define | UART_LEN_6 (1U) |
#define | UART_LEN_7 (2U) |
#define | UART_LEN_8 (3U) |
UART stop bits | |
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
#define | UART_STOPBITS_1 (0U) |
#define | UART_STOPBITS_2 (1U) |
UART Parity | |
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
#define | UART_PARITY_NONE (0x00U) |
#define | UART_PARITY_ODD (0x01U) |
#define | UART_PARITY_EVEN (0x03U) |
#define | UART_PARITY_FORCED0 (0x07U) |
#define | UART_PARITY_FORCED1 (0x05U) |
UART Flow Control Type | |
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
#define | UART_FCTYPE_NONE (0x00U) |
#define | UART_FCTYPE_HW (0x02U) |
UART Flow Control Params for RX | |
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
#define | UART_FCPARAM_RXNONE (0x00U) |
#define | UART_FCPARAM_RXXONXOFF_2 (0x01U) |
#define | UART_FCPARAM_RXXONXOFF_1 (0x02U) |
#define | UART_FCPARAM_RXXONXOFF_12 (0x03U) |
#define | UART_FCPARAM_AUTO_RTS (0x40U) |
UART Flow Control Params for TX | |
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
#define | UART_FCPARAM_TXNONE (0x00U) |
#define | UART_FCPARAM_TXXONXOFF_2 (0x04U) |
#define | UART_FCPARAM_TXXONXOFF_1 (0x08U) |
#define | UART_FCPARAM_TXXONXOFF_12 (0x0CU) |
#define | UART_FCPARAM_AUTO_CTS (0x80U) |
UART RX trigger level | |
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
#define | UART_RXTRIGLVL_1 (1U) |
#define | UART_RXTRIGLVL_8 (8U) |
#define | UART_RXTRIGLVL_16 (16U) |
#define | UART_RXTRIGLVL_56 (56U) |
#define | UART_RXTRIGLVL_60 (60U) |
UART TX trigger level | |
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
#define | UART_TXTRIGLVL_1 (1U) |
#define | UART_TXTRIGLVL_8 (8U) |
#define | UART_TXTRIGLVL_16 (16U) |
#define | UART_TXTRIGLVL_32 (32U) |
#define | UART_TXTRIGLVL_56 (56U) |
UART Operational Mode | |
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
#define | UART_OPER_MODE_16X (0U) |
#define | UART_OPER_MODE_SIR (1U) |
#define | UART_OPER_MODE_16X_AUTO_BAUD (2U) |
#define | UART_OPER_MODE_13X (3U) |
#define | UART_OPER_MODE_MIR (4U) |
#define | UART_OPER_MODE_FIR (5U) |
#define | UART_OPER_MODE_CIR (6U) |
#define | UART_OPER_MODE_DISABLED (7U) |
Values indicating the filled status of TX FIFO | |
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
#define | UART_TX_FIFO_NOT_FULL |
#define | UART_TX_FIFO_FULL |
Values related to status of Interrupt souces. | |
#define | UART_INTID_MODEM_STAT |
Values pertaining to status of UART Interrupt sources. More... | |
#define | UART_INTID_TX_THRES_REACH |
#define | UART_INTID_RX_THRES_REACH |
#define | UART_INTID_RX_LINE_STAT_ERROR |
#define | UART_INTID_CHAR_TIMEOUT |
#define | UART_INTID_XOFF_SPEC_CHAR_DETECT |
#define | UART_INTID_MODEM_SIG_STATE_CHANGE |
#define | UART_INTR_PENDING (0U) |
Values indicating the UART Interrupt pending status. More... | |
#define | UART_N0_INTR_PENDING (1U) |
Values related to enabling/disabling of Interrupts. | |
#define | UART_INTR_CTS (UART_IER_CTS_IT_MASK) |
Values for enabling/disabling the interrupts of UART. More... | |
#define | UART_INTR_RTS (UART_IER_RTS_IT_MASK) |
#define | UART_INTR_XOFF (UART_IER_XOFF_IT_MASK) |
#define | UART_INTR_SLEEPMODE (UART_IER_SLEEP_MODE_MASK) |
#define | UART_INTR_MODEM_STAT (UART_IER_MODEM_STS_IT_MASK) |
#define | UART_INTR_LINE_STAT (UART_IER_LINE_STS_IT_MASK) |
#define | UART_INTR_THR (UART_IER_THR_IT_MASK) |
#define | UART_INTR_RHR_CTI (UART_IER_RHR_IT_MASK) |
#define | UART_INTR2_RX_EMPTY (UART_IER2_EN_RXFIFO_EMPTY_MASK) |
#define | UART_INTR2_TX_EMPTY (UART_IER2_EN_TXFIFO_EMPTY_MASK) |
Values related to Line Status information. | |
#define | UART_FIFO_PE_FE_BI_DETECTED (UART_LSR_RX_FIFO_STS_MASK) |
Values pertaining to UART Line Status information. More... | |
#define | UART_BREAK_DETECTED_ERROR (UART_LSR_RX_BI_MASK) |
#define | UART_FRAMING_ERROR (UART_LSR_RX_FE_MASK) |
#define | UART_PARITY_ERROR (UART_LSR_RX_PE_MASK) |
#define | UART_OVERRUN_ERROR (UART_LSR_RX_OE_MASK) |
Values related to Register Mode Configuration. | |
#define | UART_REG_CONFIG_MODE_A ((uint32_t) 0x0080) |
Values to be used while switching between register configuration modes. More... | |
#define | UART_REG_CONFIG_MODE_B ((uint32_t) 0x00BF) |
#define | UART_REG_OPERATIONAL_MODE ((uint32_t) 0x007F) |
#define UART_FIFO_SIZE (64U) |
Uart FIFO Size.
#define UART_TRANSMITEMPTY_TRIALCOUNT (3000U) |
Timeout in ms used for TX FIFO empty at the time of delete. Three seconds is more than sufficient to transfer 64 bytes (FIFO size) at the lowest baud rate of 2400.
#define UART_ERROR_COUNT (0x00FFFFFFU) |
Count Value to check error in the recieved byte
#define UART_TRANSFER_STATUS_SUCCESS (0U) |
Transaction success.
#define UART_TRANSFER_STATUS_TIMEOUT (1U) |
Time out error.
#define UART_TRANSFER_STATUS_ERROR_BI (2U) |
Break condition error.
#define UART_TRANSFER_STATUS_ERROR_FE (3U) |
Framing error.
#define UART_TRANSFER_STATUS_ERROR_PE (4U) |
Parity error.
#define UART_TRANSFER_STATUS_ERROR_OE (5U) |
Overrun error.
#define UART_TRANSFER_STATUS_CANCELLED (6U) |
Cancelled.
#define UART_TRANSFER_STATUS_STARTED (7U) |
Transaction started.
#define UART_TRANSFER_STATUS_READ_TIMEOUT (8U) |
Read timeout error.
#define UART_TRANSFER_STATUS_ERROR_INUSE (9U) |
UART is currently in use.
#define UART_TRANSFER_STATUS_ERROR_OTH (10U) |
Other errors.
#define UART_TRANSFER_MODE_BLOCKING (0U) |
UART read/write APIs blocks execution. This mode can only be used when called within a Task context.
#define UART_TRANSFER_MODE_CALLBACK (1U) |
UART read/write APIs does not block code execution and will call a UART_CallbackFxn. This mode can be used in a Task, Swi, or Hwi context.
#define UART_READ_RETURN_MODE_FULL (0U) |
Unblock/callback when buffer is full.
#define UART_READ_RETURN_MODE_PARTIAL (1U) |
Unblock/callback when no new data comes in.
#define UART_LEN_5 (0U) |
#define UART_LEN_6 (1U) |
#define UART_LEN_7 (2U) |
#define UART_LEN_8 (3U) |
#define UART_STOPBITS_1 (0U) |
#define UART_STOPBITS_2 (1U) |
#define UART_PARITY_NONE (0x00U) |
#define UART_PARITY_ODD (0x01U) |
#define UART_PARITY_EVEN (0x03U) |
#define UART_PARITY_FORCED0 (0x07U) |
#define UART_PARITY_FORCED1 (0x05U) |
#define UART_FCTYPE_NONE (0x00U) |
#define UART_FCTYPE_HW (0x02U) |
#define UART_FCPARAM_RXNONE (0x00U) |
#define UART_FCPARAM_RXXONXOFF_2 (0x01U) |
#define UART_FCPARAM_RXXONXOFF_1 (0x02U) |
#define UART_FCPARAM_RXXONXOFF_12 (0x03U) |
#define UART_FCPARAM_AUTO_RTS (0x40U) |
#define UART_FCPARAM_TXNONE (0x00U) |
#define UART_FCPARAM_TXXONXOFF_2 (0x04U) |
#define UART_FCPARAM_TXXONXOFF_1 (0x08U) |
#define UART_FCPARAM_TXXONXOFF_12 (0x0CU) |
#define UART_FCPARAM_AUTO_CTS (0x80U) |
#define UART_RXTRIGLVL_1 (1U) |
#define UART_RXTRIGLVL_8 (8U) |
#define UART_RXTRIGLVL_16 (16U) |
#define UART_RXTRIGLVL_56 (56U) |
#define UART_RXTRIGLVL_60 (60U) |
#define UART_TXTRIGLVL_1 (1U) |
#define UART_TXTRIGLVL_8 (8U) |
#define UART_TXTRIGLVL_16 (16U) |
#define UART_TXTRIGLVL_32 (32U) |
#define UART_TXTRIGLVL_56 (56U) |
#define UART_OPER_MODE_16X (0U) |
#define UART_OPER_MODE_SIR (1U) |
#define UART_OPER_MODE_16X_AUTO_BAUD (2U) |
#define UART_OPER_MODE_13X (3U) |
#define UART_OPER_MODE_MIR (4U) |
#define UART_OPER_MODE_FIR (5U) |
#define UART_OPER_MODE_CIR (6U) |
#define UART_OPER_MODE_DISABLED (7U) |
#define UART_TX_FIFO_NOT_FULL |
#define UART_TX_FIFO_FULL |
#define UART_INTID_MODEM_STAT |
Values pertaining to status of UART Interrupt sources.
#define UART_INTID_TX_THRES_REACH |
#define UART_INTID_RX_THRES_REACH |
#define UART_INTID_RX_LINE_STAT_ERROR |
#define UART_INTID_CHAR_TIMEOUT |
#define UART_INTID_XOFF_SPEC_CHAR_DETECT |
#define UART_INTID_MODEM_SIG_STATE_CHANGE |
#define UART_INTR_PENDING (0U) |
Values indicating the UART Interrupt pending status.
#define UART_N0_INTR_PENDING (1U) |
#define UART_INTR_CTS (UART_IER_CTS_IT_MASK) |
Values for enabling/disabling the interrupts of UART.
#define UART_INTR_RTS (UART_IER_RTS_IT_MASK) |
#define UART_INTR_XOFF (UART_IER_XOFF_IT_MASK) |
#define UART_INTR_SLEEPMODE (UART_IER_SLEEP_MODE_MASK) |
#define UART_INTR_MODEM_STAT (UART_IER_MODEM_STS_IT_MASK) |
#define UART_INTR_LINE_STAT (UART_IER_LINE_STS_IT_MASK) |
#define UART_INTR_THR (UART_IER_THR_IT_MASK) |
#define UART_INTR_RHR_CTI (UART_IER_RHR_IT_MASK) |
#define UART_INTR2_RX_EMPTY (UART_IER2_EN_RXFIFO_EMPTY_MASK) |
#define UART_INTR2_TX_EMPTY (UART_IER2_EN_TXFIFO_EMPTY_MASK) |
#define UART_FIFO_PE_FE_BI_DETECTED (UART_LSR_RX_FIFO_STS_MASK) |
Values pertaining to UART Line Status information.
#define UART_BREAK_DETECTED_ERROR (UART_LSR_RX_BI_MASK) |
#define UART_FRAMING_ERROR (UART_LSR_RX_FE_MASK) |
#define UART_PARITY_ERROR (UART_LSR_RX_PE_MASK) |
#define UART_OVERRUN_ERROR (UART_LSR_RX_OE_MASK) |
#define UART_REG_CONFIG_MODE_A ((uint32_t) 0x0080) |
Values to be used while switching between register configuration modes.
#define UART_REG_CONFIG_MODE_B ((uint32_t) 0x00BF) |
#define UART_REG_OPERATIONAL_MODE ((uint32_t) 0x007F) |
typedef void* UART_Handle |
A handle that is returned from a UART_open() call.
typedef void(* UART_CallbackFxn) (UART_Handle handle, UART_Transaction *transaction) |
The definition of a callback function used by the UART driver when used in UART_TRANSFER_MODE_CALLBACK.
handle | UART_Handle |
transaction* | Pointer to a UART_Transaction |
void UART_init | ( | void | ) |
This function initializes the UART module.
void UART_deinit | ( | void | ) |
This function de-initializes the UART module.
UART_Handle UART_open | ( | uint32_t | index, |
const UART_Params * | prms | ||
) |
This function opens a given UART peripheral.
index | Index of config to use in the UART_Config array |
prms | Pointer to open parameters. If NULL is passed, then default values will be used |
void UART_close | ( | UART_Handle | handle | ) |
Function to close a UART peripheral specified by the UART handle.
handle | UART_Handle returned from UART_open() |
int32_t UART_write | ( | UART_Handle | handle, |
UART_Transaction * | trans | ||
) |
Function to perform UART write operation.
In UART_TRANSFER_MODE_BLOCKING, UART_write() will block task execution until the transaction has completed or a timeout has occurred.
In UART_TRANSFER_MODE_CALLBACK, UART_write() does not block task execution, but calls a UART_CallbackFxn once the transfer has finished. This makes UART_write() safe to be used within a Task, software or hardware interrupt context.
In interrupt mode, UART_write() does not wait until tx fifo is empty. Application needs to call UART_flushTxFifo() to ensure write is completed. i.e. data is out from the FIFO and shift registers.
From calling UART_write() until transfer completion, the UART_Transaction structure must stay persistent and must not be altered by application code. It is also forbidden to modify the content of the UART_Transaction.buf during a transaction, even though the physical transfer might not have started yet. Doing this can result in data corruption.
handle | UART_Handle returned from UART_open() |
trans | Pointer to a UART_Transaction. All of the fields within transaction except UART_Transaction.count and UART_Transaction.status are WO (write-only) unless otherwise noted in the driver implementations. If a transaction timeout has occurred, UART_Transaction.count will contain the number of bytes that were transferred. Neither is it allowed to modify the transaction object nor the content of UART_Transaction.buf until the transfer has completed |
int32_t UART_read | ( | UART_Handle | handle, |
UART_Transaction * | trans | ||
) |
Function to perform UART read operation.
In UART_TRANSFER_MODE_BLOCKING, UART_read() will block task execution until the transaction has completed or a timeout has occurred.
In UART_TRANSFER_MODE_CALLBACK, UART_read() does not block task execution, but calls a UART_CallbackFxn once the transfer has finished. This makes UART_read() safe to be used within a Task, software or hardware interrupt context.
From calling UART_read() until transfer completion, the UART_Transaction structure must stay persistent and must not be altered by application code. It is also forbidden to modify the content of the UART_Transaction.buf during a transaction, even though the physical transfer might not have started yet. Doing this can result in data corruption.
handle | UART_Handle returned from UART_open() |
trans | Pointer to a UART_Transaction. All of the fields within transaction except UART_Transaction.count and UART_Transaction.status are WO (write-only) unless otherwise noted in the driver implementations. If a transaction timeout has occurred, UART_Transaction.count will contain the number of bytes that were transferred. Neither is it allowed to modify the transaction object nor the content of UART_Transaction.buf until the transfer has completed |
int32_t UART_writeCancel | ( | UART_Handle | handle, |
UART_Transaction * | trans | ||
) |
Function to perform UART canceling of current write transaction.
In UART_TRANSFER_MODE_CALLBACK, UART_writeCancel() does not block task execution, but calls a UART_CallbackFxn once the cancel has finished. This makes UART_writeCancel() safe to be used within a Task, software or hardware interrupt context.
From calling UART_writeCancel() until cancel completion, the UART_Transaction structure must stay persistent and must not be altered by application code. It is also forbidden to modify the content of the UART_Transaction.buf during a transaction, even though the physical transfer might not have started yet. Doing this can result in data corruption.
handle | UART_Handle returned from UART_open() |
trans | Pointer to a UART_Transaction. All of the fields within transaction except UART_Transaction.count and UART_Transaction.status are WO (write-only) unless otherwise noted in the driver implementations. If a transaction timeout has occurred, UART_Transaction.count will contain the number of bytes that were transferred. Neither is it allowed to modify the transaction object nor the content of UART_Transaction.buf until the transfer has completed |
int32_t UART_readCancel | ( | UART_Handle | handle, |
UART_Transaction * | trans | ||
) |
Function to perform UART canceling of current read transaction.
In UART_TRANSFER_MODE_CALLBACK, UART_readCancel() does not block task execution, but calls a UART_CallbackFxn once the cancel has finished. This makes UART_writeCancel() safe to be used within a Task, software or hardware interrupt context.
From calling UART_readCancel() until cancel completion, the UART_Transaction structure must stay persistent and must not be altered by application code. It is also forbidden to modify the content of the UART_Transaction.buf during a transaction, even though the physical transfer might not have started yet. Doing this can result in data corruption.
handle | UART_Handle returned from UART_open() |
trans | Pointer to a UART_Transaction. All of the fields within transaction except UART_Transaction.count and UART_Transaction.status are WO (write-only) unless otherwise noted in the driver implementations. If a transaction timeout has occurred, UART_Transaction.count will contain the number of bytes that were transferred. Neither is it allowed to modify the transaction object nor the content of UART_Transaction.buf until the transfer has completed |
UART_Handle UART_getHandle | ( | uint32_t | index | ) |
Function to return a open'ed UART handle given a UART instance index.
index | Index of config to use in the UART_Config array |
void UART_flushTxFifo | ( | UART_Handle | handle | ) |
Function to flush a TX FIFO of peripheral specified by the UART handle.
handle | UART_Handle returned from UART_open() |
|
inlinestatic |
Function to initialize the UART_Params struct to its defaults.
prms | Pointer to UART_Params structure for initialization |
|
inlinestatic |
Function to initialize the UART_Transaction struct to its defaults.
trans | Pointer to UART_Transaction structure for initialization |
uint32_t UART_getBaseAddr | ( | UART_Handle | handle | ) |
Function to get base address of UART instance of a particular handle.
handle | UART_Handle returned from UART_open() |
void UART_enableLoopbackMode | ( | uint32_t | baseAddr | ) |
Function to enable loopback mode. This function is for internal use. Not recommended for customers to use.
baseAddr | Memory address of the UART instance being used. |
void UART_disableLoopbackMode | ( | uint32_t | baseAddr | ) |
Function to disable loopback mode. This function is for internal use. Not recommended for customers to use.
baseAddr | Memory address of the UART instance being used. |
|
inlinestatic |
This API writes a byte to the Transmitter FIFO without checking for the emptiness of the Transmitter FIFO or the Transmitter Shift Register(TSR).
baseAddr | Memory address of the UART instance being used. |
byteTx | The byte to be transmitted by the UART. |
|
inlinestatic |
This API reads a byte from the Receiver Buffer Register (RBR). It checks once if any character is ready to be read.
baseAddr | Memory address of the UART instance being used. |
pChar | Pointer to the byte variable which saves the byte read from RBR if there is any char ready to be read |
|
inlinestatic |
This API enables the specified interrupts in the UART mode of operation.
baseAddr | Memory address of the UART instance being used. |
intrFlag | Bit mask value of the bits corresponding to Interrupt Enable Register(IER). This specifies the UART interrupts to be enabled. |
'intrFlag' can take one or a combination of the following macros:
|
inlinestatic |
This API disables the specified interrupts in the UART mode of operation.
baseAddr | Memory address of the UART instance being used. |
intrFlag | Bit mask value of the bits corresponding to Interrupt Enable Register(IER). This specifies the UART interrupts to be disabled. |
'intrFlag' can take one or a combination of the following macros:
|
inlinestatic |
This API enables the specified interrupts in the UART mode of operation for IER2.
baseAddr | Memory address of the UART instance being used. |
intrFlag | Bit mask value of the bits corresponding to Interrupt Enable Register(IER2). This specifies the UART interrupts to be enabled. |
'intrFlag' can take one or a combination of the following macros:
|
inlinestatic |
This API disables the specified interrupts in the UART mode of operation for IER2.
baseAddr | Memory address of the UART instance being used. |
intrFlag | Bit mask value of the bits corresponding to Interrupt Enable Register(IER2). This specifies the UART interrupts to be disabled. |
'intrFlag' can take one or a combination of the following macros:
|
inlinestatic |
This API determines the UART Interrupt Status.
baseAddr | Memory address of the UART instance being used. |
|
inlinestatic |
This API determines the UART Interrupt Status 2.
baseAddr | Memory address of the UART instance being used. |
|
inlinestatic |
This API checks if the RX FIFO (or RHR in non-FIFO mode) has atleast one byte of data to be read.
baseAddr | Memory address of the UART instance being used. |
|
inlinestatic |
This API reads the line status register value.
baseAddr | Memory address of the UART instance being used. |
|
inlinestatic |
This API reads the data present at the top of the RX FIFO, that is, the data in the Receive Holding Register(RHR). However before reading the data from RHR, it checks for RX error.
baseAddr | Memory address of the UART instance being used. |
readBuf | Pointer to the byte buffer to be read from RHR register. |
|
extern |
Externally defined driver configuration array.
|
extern |
Externally defined driver configuration array size.