This section describes the differences between UART APIs of MCU+ SDK and Processor SDK RTOS (PDK). This can be used as a migration aid when moving from Processor SDK RTOS (PDK) to MCU+ SDK.
In MCU+ SDK, the UART module provides higher level driver APIs.Refer UART for more details.
There are changes in functions names, structure names and macro names. The changes in function names are listed below.
PDK | MCU+ SDK | Change Description / Remarks |
---|---|---|
UART_init | UART_init | NO CHANGE |
None | UART_deinit | In MCU+SDK, this API can be used to de-initialize the UART module. |
UART_open | UART_open | NO CHANGE |
UART_close | UART_close | NO CHANGE |
UART_write | UART_write | NO CHANGE |
UART_read | UART_read | NO CHANGE |
UART_writeCancel | UART_writeCancel | NO CHANGE |
UART_readCancel | UART_readCancel | NO CHANGE |
None | UART_getHandle | In MCU+SDK, this API can be used to get the handle of an open UART instance from the instance index. |
None | UART_flushTxFifo | In MCU+SDK, this API is used to flush a TX FIFO of peripheral specified by the UART handle |
UART_Params_init | UART_Params_init | NO CHANGE |
UART_transactionInit | UART_Transaction_init | API rename |
UART_control | None | This is a dummy function in PDK also. |
UART_writePolling | UART_write | Configuring field UART_Params::intrEnable to Polled mode will do the equivalent of PDK UART API. |
UART_readPolling | UART_read | Configuring field UART_Params::intrEnable to Polled mode will do the equivalent of PDK UART API. |
UART_read2 | UART_read | API rename |
UART_write2 | UART_write | API rename |