Go to the source code of this file.
Data Structures | |
struct | ClockP_Object |
Opaque clock object used with the clock APIs. More... | |
struct | ClockP_Config |
ClockP module config, set as part of SysConfig, not to be set by end-users directly. More... | |
struct | ClockP_Params |
Parameters passed during ClockP_construct. More... | |
Macros | |
#define | ClockP_OBJECT_SIZE_MAX (64u) |
Max size of clock object across no-RTOS and all OS's. More... | |
Typedefs | |
typedef void(* | ClockP_FxnCallback) (ClockP_Object *obj, void *args) |
Callback that is called when the clock expires. More... | |
Functions | |
void | ClockP_init () |
Initialize the clock module. More... | |
void | ClockP_Params_init (ClockP_Params *params) |
Set default values to ClockP_Params. More... | |
int32_t | ClockP_construct (ClockP_Object *obj, ClockP_Params *params) |
Create a clock object. More... | |
void | ClockP_destruct (ClockP_Object *obj) |
Cleanup, delete, destruct a clock object. More... | |
void | ClockP_start (ClockP_Object *obj) |
Start the clock, if not already started. More... | |
void | ClockP_stop (ClockP_Object *obj) |
Stop the clock, if not already stopped. No effect if clock is already stopped. More... | |
uint32_t | ClockP_isActive (ClockP_Object *obj) |
Check if clock is active i.e not expired. More... | |
void | ClockP_setTimeout (ClockP_Object *obj, uint32_t timeout) |
Set clock timeout value, takes effect for next clock start. More... | |
uint32_t | ClockP_getTimeout (ClockP_Object *obj) |
Get current remaining time in units of ticks. More... | |
uint32_t | ClockP_getTicks () |
Get current clock ticks. More... | |
uint32_t | ClockP_usecToTicks (uint64_t usecs) |
Convert usecs to clock ticks. More... | |
uint64_t | ClockP_ticksToUsec (uint32_t ticks) |
Convert clock ticks to usecs. More... | |
uint64_t | ClockP_getTimeUsec () |
Get current time in units of usecs. More... | |
void | ClockP_usleep (uint32_t usec) |
Sleep for user specified usecs. More... | |
void | ClockP_sleep (uint32_t sec) |
Sleep for user specified seconds. More... | |