uint32_t EI_API_ADP_getIpAddr | ( | T * | pAdp_p, |
uint32_t * | pIpAddr_p | ||
) |
Get the IP address of the selected adapter (Instance Attribute ID: 5).
Function that returns the IP address of the adapter selected by parameter pAdp_p
in output parameter pIpAddr_p
.
[in] | pAdp_p | Pointer to the adapter. |
[out] | pIpAddr_p | uint32_t pointer to IP address of the adapter specified by parameter pAdp_p . |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |