uint32_t EI_API_ADP_getProductCode | ( | T * | pAdp_p, |
uint16_t * | pProductCode_p | ||
) |
Get the adapter product code (Instance Attribute ID: 3).
Function that returns the product code of the adapter selected by parameter pAdp_p
.
[in] | pAdp_p | Pointer to the adapter. |
[out] | pProductCode_p | Pointer to the product code. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |