uint32_t EI_API_ADP_getModuleNetworkStatus | ( | T * | pAdp_p, |
EI_API_ADP_SModNetStatus_t * | pAdpStatus_p | ||
) |
Get adapter status values.
This function may be called to retrieve module and network status values from the adapter.
[in] | pAdp_p | Pointer to the adapter. |
[out] | pAdpStatus_p | Pointer of type EI_API_ADP_SModNetStatus_t to the adapter status structure. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |