EtherCAT Slave  1.04.01

◆ EC_API_SLV_FoE_cbRegisterReadFileHandler()

void EC_API_SLV_FoE_cbRegisterReadFileHandler ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
void *  pContext_p,
EC_API_SLV_FoE_CBReadFileHandler_t  cbFunc_p 
)

This is the function to register FoE read function.

This function registers a function pointer which must be implemented by the user. The user defined function will be called if a file read request is received from the master.

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
[in]pContext_preadFileHandler call context
[in]cbFunc_pcbFunc Function pointer to the FoE Read file
Example
#include <ecSlvApi.h>
// the Call
EC_API_SLV_FoE_cbRegisterReadFileHandler(ecSlaveApi, ecSlaveApi, cbFunc);
EC_API_SLV_FoE_cbRegisterReadFileHandler
void EC_API_SLV_FoE_cbRegisterReadFileHandler(EC_API_SLV_SHandle_t *pEcSlaveApi_p, void *pContext_p, EC_API_SLV_FoE_CBReadFileHandler_t cbFunc_p)
This is the function to register FoE read function.
Definition: ecSlvApi_FoEStub.c:124