AM243x MCU+ SDK  08.00.00
MCSPI_OpenParams Struct Reference

Detailed Description

MCSPI Parameters.

MCSPI Parameters are used to with the MCSPI_open() call. Default values for these parameters are set using MCSPI_OpenParams_init().

If NULL is passed for the parameters, MCSPI_open() uses default parameters.

See also
MCSPI_OpenParams_init()

Data Fields

uint32_t transferMode
 
uint32_t transferTimeout
 
MCSPI_CallbackFxn transferCallbackFxn
 
uint32_t msMode
 

Field Documentation

◆ transferMode

uint32_t MCSPI_OpenParams::transferMode

Blocking or Callback mode. Refer MCSPI_TransferMode

◆ transferTimeout

uint32_t MCSPI_OpenParams::transferTimeout

Transfer timeout in system ticks

◆ transferCallbackFxn

MCSPI_CallbackFxn MCSPI_OpenParams::transferCallbackFxn

Callback function pointer

◆ msMode

uint32_t MCSPI_OpenParams::msMode

Master or Slave mode. Refer MCSPI_MsMode