Structure holding the Event Trigger Sub-Module configuration parameters.
Data Fields | |
uint32_t | intrEvtSource |
uint32_t | intrPrd |
uint32_t Epwm_EtCfg_t::intrEvtSource |
Event which is the source of the interrupt. This can take values from the following enum Epwm_EtIntrEvt_t.
uint32_t Epwm_EtCfg_t::intrPrd |
Interrupt period which determine how many selected events need to occur before an interrupt is generated. This can take values from the following enum Epwm_EtIntrPeriod_t.