This module contains APIs to program and use the Ethernet PHY present on the board. See ETHPHY for more details.
Data Structures | |
struct | ETHPHY_Params |
Parameters passed during ETHPHY_open() More... | |
struct | ETHPHY_Fxns |
ETHPHY Driver implementation callbacks. More... | |
struct | ETHPHY_Attrs |
ETHPHY device attributes. These are filled by SysCfg based on the PHY device that is selected. More... | |
struct | ETHPHY_Config |
ETHPHY driver configuration. These are filled by SysCfg based on the PHY device that is selected. More... | |
struct | ETHPHY_SpeedDuplexConfig |
Data structure to be passed/returned when calling ETHPHY_command with ETHPHY_CMD_GET_SPEED_AND_DUPLEX_CONFIG or ETHPHY_CMD_SET_SPEED_AND_DUPLEX_CONFIG. More... | |
Functions | |
void | ETHPHY_Params_init (ETHPHY_Params *params) |
Set default parameters in the ETHPHY_Params structure. More... | |
ETHPHY_Handle | ETHPHY_open (uint32_t instanceId, const ETHPHY_Params *params) |
Open ETHPHY driver. More... | |
void | ETHPHY_close (ETHPHY_Handle handle) |
Close ETHPHY driver. More... | |
int32_t | ETHPHY_command (ETHPHY_Handle handle, uint32_t command, void *data, uint32_t dataSize) |
Send a command to the ETHPHY. More... | |
const ETHPHY_Attrs * | ETHPHY_getAttrs (uint32_t instanceId) |
Return ETHPHY attributes. More... | |
Typedefs | |
typedef void * | ETHPHY_Handle |
Handle to the ETHPHY driver returned by ETHPHY_open() More... | |
typedef struct ETHPHY_Config_s | ETHPHY_Config |
Forward declaration of ETHPHY_Config. More... | |
typedef struct ETHPHY_Params_s | ETHPHY_Params |
Forward declaration of ETHPHY_Params. More... | |
ETHPHY Commands | |
Various commands for the Eternet PHY | |
#define | ETHPHY_CMD_ENABLE_MII (0U) |
Command to configure the PHY in MII mode. More... | |
#define | ETHPHY_CMD_SOFT_RESTART (1U) |
Command for Soft Restart. It restarts the PHY without affecting registers. More... | |
#define | ETHPHY_CMD_ENABLE_AUTO_MDIX (2U) |
Command to enable Auto MDI-X (Automatic Crossover) More... | |
#define | ETHPHY_CMD_VERIFY_IDENTIFIER_REGISTER (3U) |
Command to verify the PHY Identifier Register. It checks if the PHYIDR1 register has the expected value. More... | |
#define | ETHPHY_CMD_DISABLE_1000M_ADVERTISEMENT (4U) |
Command to disable 1000M ability advertisement More... | |
#define | ETHPHY_CMD_ENABLE_FAST_LINK_DOWN_DETECTION (5U) |
Command to enable Fast Link Down Detection. "data" argument should be passed while making ETHPHY_command API call with this command. Refer to the PHY-specific .h file in "source/board/ethphy" for the data structure needed to be passed. More... | |
#define | ETHPHY_CMD_CONFIGURE_LED_SOURCE (6U) |
Command to configure the source of PHY LEDs. "data" argument should be passed while making ETHPHY_command API call with this command. Refer to the PHY-specific .h file in "source/board/ethphy" for the data structure needed to be passed. More... | |
#define | ETHPHY_CMD_CONFIGURE_LED_BLINK_RATE (7U) |
Command to configure the blink rate of PHY LEDs. "data" argument should be passed while making ETHPHY_command API call with this command. Refer to the PHY-specific .h file in "source/board/ethphy" for the data structure needed to be passed. More... | |
#define | ETHPHY_CMD_ENABLE_EXTENDED_FD_ABILITY (8U) |
Command to enable the extended full duplex ability. More... | |
#define | ETHPHY_CMD_ENABLE_ODD_NIBBLE_DETECTION (9U) |
Command to enable odd nibble detection. More... | |
#define | ETHPHY_CMD_ENABLE_ENHANCED_IPG_DETECTION (10U) |
Command to enable enhanced IPG detection. More... | |
#define | ETHPHY_CMD_GET_LINK_STATUS (11U) |
Command to get Link Status for the PHY. More... | |
#define | ETHPHY_CMD_GET_SPEED_AND_DUPLEX_CONFIG (12U) |
Command to get Speed and Duplex configuration for the PHY. "data" argument should be passed while making ETHPHY_command API call with this command. "data" should be of type ETHPHY_SpeedDuplexConfig. More... | |
#define | ETHPHY_CMD_SET_SPEED_AND_DUPLEX_CONFIG (13U) |
Command to set Speed and Duplex configuration for the PHY. "data" argument should be passed while making ETHPHY_command API call with this command. "data" should be of type ETHPHY_SpeedDuplexConfig. More... | |
#define | ETHPHY_CMD_ENABLE_LOW_LATENCY_10M_100M_RGMII (14U) |
Command to enable low latency for 10M/100M operation in RGMII mode. More... | |
#define | ETHPHY_CMD_SET_RX_HALF_FULL_THRESHOLD_RGMII (15U) |
Command to set RX half full threshold in RGMII mode. "data" argument should be passed while making ETHPHY_command API call with this command. "data" should be a pointer to "uint8_t" and value should be present in the lowest 3 bits. More... | |
#define | ETHPHY_CMD_SET_TX_HALF_FULL_THRESHOLD_RGMII (16U) |
Command to set TX half full threshold in RGMII mode. "data" argument should be passed while making ETHPHY_command API call with this command. "data" should be a pointer to "uint8_t" and value should be present in the lowest 3 bits. More... | |
#define | ETHPHY_CMD_GET_AUTONEG_COMPLETE_STATUS (17U) |
Command to get auto-negotiation completion status. "data" argument should be passed while making ETHPHY_command API call with this command. "data" should be a pointer to "uint8_t" and value returned will be 0 if auto-negotiation is not complete, and 1 if it is complete. More... | |
#define | ETHPHY_CMD_GET_LINK_PARTNER_AUTONEG_ABILITY (18U) |
Command to get link partner's auto-negotiation ability. "data" argument should be passed while making ETHPHY_command API call with this command. "data" should be a pointer to "uint8_t" and value returned will be 0 if partner is not auto-negotiation able, and 1 if it is in auto-neogtiation able. More... | |
ETHPHY SPEED AND DUPLEX CONFIGURATIONS | |
Different modes for speed and duplex configuration in ETHPHY | |
#define | ETHPHY_SPEED_DUPLEX_CONFIG_AUTONEG (0U) |
#define | ETHPHY_SPEED_DUPLEX_CONFIG_10FD (1U) |
#define | ETHPHY_SPEED_DUPLEX_CONFIG_100FD (2U) |
#define | ETHPHY_SPEED_DUPLEX_CONFIG_1000FD (3U) |
#define | ETHPHY_SPEED_DUPLEX_CONFIG_10HD (4U) |
#define | ETHPHY_SPEED_DUPLEX_CONFIG_100HD (5U) |
#define | ETHPHY_SPEED_DUPLEX_CONFIG_1000HD (6U) |
#define | ETHPHY_SPEED_DUPLEX_CONFIG_INVALID (7U) |
ETHPHY driver implementation callbacks | |
typedef int32_t(* | ETHPHY_OpenFxn) (ETHPHY_Config *config, const ETHPHY_Params *params) |
Driver implementation to open a specific ETHPHY driver. More... | |
typedef void(* | ETHPHY_CloseFxn) (ETHPHY_Config *config) |
Driver implementation to close a specific ETHPHY driver. More... | |
typedef int32_t(* | ETHPHY_CommandFxn) (ETHPHY_Config *config, uint32_t command, void *data, uint32_t dataSize) |
Driver implementation to send command to the ETHPHY using specific ETHPHY driver. More... | |
#define ETHPHY_CMD_ENABLE_MII (0U) |
Command to configure the PHY in MII mode.
#define ETHPHY_CMD_SOFT_RESTART (1U) |
Command for Soft Restart. It restarts the PHY without affecting registers.
#define ETHPHY_CMD_ENABLE_AUTO_MDIX (2U) |
Command to enable Auto MDI-X (Automatic Crossover)
#define ETHPHY_CMD_VERIFY_IDENTIFIER_REGISTER (3U) |
Command to verify the PHY Identifier Register. It checks if the PHYIDR1 register has the expected value.
#define ETHPHY_CMD_DISABLE_1000M_ADVERTISEMENT (4U) |
Command to disable 1000M ability advertisement
#define ETHPHY_CMD_ENABLE_FAST_LINK_DOWN_DETECTION (5U) |
Command to enable Fast Link Down Detection. "data" argument should be passed while making ETHPHY_command API call with this command. Refer to the PHY-specific .h file in "source/board/ethphy" for the data structure needed to be passed.
#define ETHPHY_CMD_CONFIGURE_LED_SOURCE (6U) |
Command to configure the source of PHY LEDs. "data" argument should be passed while making ETHPHY_command API call with this command. Refer to the PHY-specific .h file in "source/board/ethphy" for the data structure needed to be passed.
#define ETHPHY_CMD_CONFIGURE_LED_BLINK_RATE (7U) |
Command to configure the blink rate of PHY LEDs. "data" argument should be passed while making ETHPHY_command API call with this command. Refer to the PHY-specific .h file in "source/board/ethphy" for the data structure needed to be passed.
#define ETHPHY_CMD_ENABLE_EXTENDED_FD_ABILITY (8U) |
Command to enable the extended full duplex ability.
#define ETHPHY_CMD_ENABLE_ODD_NIBBLE_DETECTION (9U) |
Command to enable odd nibble detection.
#define ETHPHY_CMD_ENABLE_ENHANCED_IPG_DETECTION (10U) |
Command to enable enhanced IPG detection.
#define ETHPHY_CMD_GET_LINK_STATUS (11U) |
Command to get Link Status for the PHY.
#define ETHPHY_CMD_GET_SPEED_AND_DUPLEX_CONFIG (12U) |
Command to get Speed and Duplex configuration for the PHY. "data" argument should be passed while making ETHPHY_command API call with this command. "data" should be of type ETHPHY_SpeedDuplexConfig.
#define ETHPHY_CMD_SET_SPEED_AND_DUPLEX_CONFIG (13U) |
Command to set Speed and Duplex configuration for the PHY. "data" argument should be passed while making ETHPHY_command API call with this command. "data" should be of type ETHPHY_SpeedDuplexConfig.
#define ETHPHY_CMD_ENABLE_LOW_LATENCY_10M_100M_RGMII (14U) |
Command to enable low latency for 10M/100M operation in RGMII mode.
#define ETHPHY_CMD_SET_RX_HALF_FULL_THRESHOLD_RGMII (15U) |
Command to set RX half full threshold in RGMII mode. "data" argument should be passed while making ETHPHY_command API call with this command. "data" should be a pointer to "uint8_t" and value should be present in the lowest 3 bits.
#define ETHPHY_CMD_SET_TX_HALF_FULL_THRESHOLD_RGMII (16U) |
Command to set TX half full threshold in RGMII mode. "data" argument should be passed while making ETHPHY_command API call with this command. "data" should be a pointer to "uint8_t" and value should be present in the lowest 3 bits.
#define ETHPHY_CMD_GET_AUTONEG_COMPLETE_STATUS (17U) |
Command to get auto-negotiation completion status. "data" argument should be passed while making ETHPHY_command API call with this command. "data" should be a pointer to "uint8_t" and value returned will be 0 if auto-negotiation is not complete, and 1 if it is complete.
#define ETHPHY_CMD_GET_LINK_PARTNER_AUTONEG_ABILITY (18U) |
Command to get link partner's auto-negotiation ability. "data" argument should be passed while making ETHPHY_command API call with this command. "data" should be a pointer to "uint8_t" and value returned will be 0 if partner is not auto-negotiation able, and 1 if it is in auto-neogtiation able.
#define ETHPHY_SPEED_DUPLEX_CONFIG_AUTONEG (0U) |
#define ETHPHY_SPEED_DUPLEX_CONFIG_10FD (1U) |
#define ETHPHY_SPEED_DUPLEX_CONFIG_100FD (2U) |
#define ETHPHY_SPEED_DUPLEX_CONFIG_1000FD (3U) |
#define ETHPHY_SPEED_DUPLEX_CONFIG_10HD (4U) |
#define ETHPHY_SPEED_DUPLEX_CONFIG_100HD (5U) |
#define ETHPHY_SPEED_DUPLEX_CONFIG_1000HD (6U) |
#define ETHPHY_SPEED_DUPLEX_CONFIG_INVALID (7U) |
typedef void* ETHPHY_Handle |
Handle to the ETHPHY driver returned by ETHPHY_open()
typedef struct ETHPHY_Config_s ETHPHY_Config |
Forward declaration of ETHPHY_Config.
typedef struct ETHPHY_Params_s ETHPHY_Params |
Forward declaration of ETHPHY_Params.
typedef int32_t(* ETHPHY_OpenFxn) (ETHPHY_Config *config, const ETHPHY_Params *params) |
Driver implementation to open a specific ETHPHY driver.
Typically this callback is hidden from the end application and is implemented when a new type of ETHPHY device needs to be implemented.
config | [IN] ETHPHY configuration for the specific ETHPHY device |
params | [IN] User controllable parameters when opening the ETHPHY device |
typedef void(* ETHPHY_CloseFxn) (ETHPHY_Config *config) |
Driver implementation to close a specific ETHPHY driver.
Typically this callback is hidden from the end application and is implemented when a new type of ETHPHY device needs to be implemented.
config | [IN] ETHPHY configuration for the specific ETHPHY device |
typedef int32_t(* ETHPHY_CommandFxn) (ETHPHY_Config *config, uint32_t command, void *data, uint32_t dataSize) |
Driver implementation to send command to the ETHPHY using specific ETHPHY driver.
Typically this callback is hidden from the end application and is implemented when a new type of ETHPHY device needs to be implemented.
config | [IN] ETHPHY configuration for the specific ETHPHY device |
command | [IN] Command from ETHPHY_Commands |
data | [IN] Pointer to structure which has the data to write/read |
dataSize | [IN] Size of the structure pointed by data |
void ETHPHY_Params_init | ( | ETHPHY_Params * | params | ) |
Set default parameters in the ETHPHY_Params structure.
Call this API to set defaults and then override the fields as needed before calling ETHPHY_open.
params | [OUT] Initialized parameters |
ETHPHY_Handle ETHPHY_open | ( | uint32_t | instanceId, |
const ETHPHY_Params * | params | ||
) |
Open ETHPHY driver.
Global variables ETHPHY_Config gETHPHY_Config[]
and uint32_t gETHPHY_ConfigNum
is instantiated by SysCfg to describe the ETHPHY configuration based on user selection in SysCfg.
instanceId | [IN] Index within ETHPHY_Config gETHPHY_Config[] denoting the ETHPHY driver to open |
params | [IN] Open parameters |
void ETHPHY_close | ( | ETHPHY_Handle | handle | ) |
Close ETHPHY driver.
handle | [in] ETHPHY driver handle from ETHPHY_open |
int32_t ETHPHY_command | ( | ETHPHY_Handle | handle, |
uint32_t | command, | ||
void * | data, | ||
uint32_t | dataSize | ||
) |
Send a command to the ETHPHY.
handle | [in] ETHPHY driver handle from ETHPHY_open |
command | [in] Command from ETHPHY_Commands |
data | [IN] Pointer to structure which has the data to write/read |
dataSize | [IN] Size of the structure pointed by data |
const ETHPHY_Attrs* ETHPHY_getAttrs | ( | uint32_t | instanceId | ) |
Return ETHPHY attributes.
instanceId | [IN] ETHPHY instance ID |