1. Installing the Compiler¶
Note
The typical use model for the compiler is to invoke it from within EdgeAI Studio Model Composer. The following steps are required only if the compiler is used directly from the command-line.
1.1. Installing¶
TI Neural Network Compiler for MCUs is distributed as a prebuilt Python package in wheel format for either Linux or Windows. Using a Python 3.10 virtual environment is recommended. Install the package using the standard Python wheel installation mechanism. For example:
Linux/Windows
pip3 install --extra-index-url https://software-dl.ti.com/mctools/esd/tvm/mcu ti_mcu_nnc
By default, the above command installs the latest ti_mcu_nnc release. You can use the ==
operator to install a specific version, for example, ti_mcu_nnc==2.0.0.
Note
Please make sure the Python virtual environment path does not contain spaces.
1.2. Verifying Install¶
After installation, verify that the compiler is available as follows:
Linux
pip3 show ti_mcu_nnc which tvmc python3 -c "import tvm; print(tvm.__file__)" ls `python3 -c "import tvm; print(tvm.__path__[0])"`/ti_docs/index.htmlWindows Git BASH
pip3 show ti_mcu_nnc which tvmc python -c "import tvm; print(tvm.__file__)" ls `python -c "import tvm; print(tvm.__path__[0])"`/ti_docs/index.htmlWindows PowerShell
pip3 show ti_mcu_nnc get-command tvmc python -c "import tvm; print(tvm.__file__)"
A local copy of the user guide is also available in the installation, inside the ti_docs directory.
TI Neural Network Compiler (NNC) for MCUs is built on top of Apache TVM, hence you will see “tvmc” as the compiler command name and “tvm” as the installation directory name.
1.3. Tested Platforms¶
Ubuntu 22.04, Python 3.10
Windows 10/11, Python 3.10