12. Frequently Asked Questions (FAQs)ΒΆ
Q: How to resolve the following error message when compiling an ONNX model exported from PyTorch?
ERROR:TVMC: dynamic shape not supported.
A: This error could be caused by exporting a PyTorch model with dynamic input and output shapes. For example, if your
torch.onnx.export()call contains adynamic_axesargument, remove it.Q: How to compile models in Keras(.h5) format via TFLite conversion for F29x devices?
A: We recommend using
TFLiteConverterutility in tensorflow python package to convert the model into TFLite format first, and then compiling the TFLite model.We do not recommend this path for non-F29x devices, for example, C28x/TI-NPU based devices, as we do not support TI-NPU QAT for Keras.
# pip install tensorflow from tensorflow import lite from tensorflow import keras h5_model = keras.models.load_model("./model.h5") converter = lite.TFLiteConverter.from_keras_model(h5_model) tflite_model = converter.convert() with open("model.tflite", "wb") as f: f.write(tflite_model)