Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
SHA2.h File Reference

Detailed Description

SHA2 driver header.

============================================================================

Warning
This is a beta API. It may change in future releases.

Overview

SHA2 (Secure Hash Algorithm 2) is a cryptographic hashing algorithm that maps an input of arbitrary length to a fixed-length output with negligible probability of collision.

It is not currently technologicaly feasible to derive an input from the hash itself.

Hashes are often used to ensure the integrity of messages. They are also used to as constituent parts of more complicated cyptographic schemes. HMAC is a message authentication code that is based on hash functions such as SHA2 rather than a block cipher. Hashes may themselves be used as or form a part of key derivation functions used to derive symmetric keys from sources of entropy such as an Elliptic Curve Diffie-Helman key exchange (ECDH).

SHA2 is not actually a single algorithms but a suite of similar algorithms that produce hashes of different lengths. 224, 256, 384, and 512-bit outputs are available.

Usage

Before starting a SHA2 operation

Before starting a SHA2 operation, the application must do the following:

Starting a SHA2 operation

There are two general ways to execute a SHA2 operation. In one call or multiple.

The SHA2_oneStepHash function performs a SHA2 operation in a single call. It will always be the most highly optimized routine with the least overhead and the fastest runtime. However, it requires that the entire input message be available to the function at the start of the call. When trying to operate on data that is too large to fit into available memory, partial processing would be more advisable. The single call operation is required when hashing a message with lenth smaller than or equal to one hash-block length. All devices support single call operations.

After the SHA2 operation completes

After the SHA2 operation completes, the application should either start another operation or close the driver by calling SHA2_close()

SHA2 Driver Configuration

In order to use the SHA2 APIs, the application is required to provide device-specific SHA2 configuration in the Board.c file. The SHA2 driver interface defines a configuration data structure:

typedef struct SHA2_Config_ {
void *object;
void const *hwAttrs;

The application must declare an array of SHA2_Config elements, named SHA2_config[]. Each element of SHA2_config[] must be populated with pointers to a device specific SHA2 driver implementation's driver object and hardware attributes. The hardware attributes define properties such as the SHA2 peripheral's base address. Each element in SHA2_config[] corresponds to an SHA2 instance and none of the elements should have NULL pointers. There is no correlation between the index and the peripheral designation (such as SHA20 or SHA21). For example, it is possible to use SHA2_config[0] for SHA21. Multiple drivers and driver instances may all access the same underlying hardware. This is transparent to the application. Mutual exclusion is performed automatically by the drivers as necessary.

Because the SHA2 configuration is very device dependent, you will need to check the doxygen for the device specific SHA2 implementation. There you will find a description of the SHA2 hardware attributes. Please also refer to the Board.c file of any of your examples to see the SHA2 configuration.

SHA2 Parameters

The SHA2_Params structure is passed to the SHA2_open() call. If NULL is passed for the parameters, SHA2_open() uses default parameters. A SHA2_Params structure is initialized with default values by passing it to SHA2_Params_init(). Some of the SHA2 parameters are described below. To see brief descriptions of all the parameters, see SHA2_Params.

Examples

### Single call SHA2 256=bit hash in blocking mode

SHA2_Handle handle;
HA2_OperationOneStepHash operationOneStepHash;
uint8_t message[] = ""; // The message is the empty string
handle = SHA2_open(0, NULL);
if (!handle) {
while(1);
}
SHA2_OperationOneStepHash_init(&operationOneStepHash);
operationOneStepHash.hashSize = SHA2_HASH_SIZE_256;
operationOneStepHash.message = message;
operationOneStepHash.digest = digest;
operationOneStepHash.totalLength = 0;
int_fast16_t testResult = SHA2_oneStepHash(handle, &operationOneStepHash);
if (testResult != SHA2_STATUS_SUCCESS) {
// handle error
while(1);
}
// The resultant digest should be:
// 0xE3, 0xB0, 0xC4, 0x42,
// 0x98, 0xFC, 0x1C, 0x14,
// 0x9A, 0xFB, 0xF4, 0xC8,
// 0x99, 0x6F, 0xB9, 0x24,
// 0x27, 0xAE, 0x41, 0xE4,
// 0x64, 0x9B, 0x93, 0x4C,
// 0xA4, 0x95, 0x99, 0x1B,
// 0x78, 0x52, 0xB8, 0x55,
SHA2_close(handle);

Partial hash with exported intermediate context

SHA2_Handle handle;
HA2_OperationStartHash operationStartHash;
HA2_OperationFinishHash operationFinishHash;
// 112-byte string
uint8_t message[] = "abcdefghbcdefghicdefghijdefghijkefghijklfghijklmgh
ijklmnhijklmnoijklmnopjklmnopqklmnopqrlmnopqrsmnop
qrstnopqrstu";
handle = SHA2_open(0, NULL);
if (!handle) {
while(1);
}
SHA2_OperationStartHash_init(&operationStartHash);
operationStartHash.hashSize = SHA2_HASH_SIZE_256;
operationStartHash.length = SHA2_DIGEST_LENGTH_BYTES_256;
operationStartHash.message = message;
operationStartHash.intermediateDigest = digest;
int_fast16_t testResult = SHA2_startHash(handle, &operationStartHash);
if (testResult != SHA2_STATUS_SUCCESS) {
while(1);
}
SHA2_OperationFinishHash_init(&operationFinishHash);
operationFinishHash.hashSize = SHA2_HASH_SIZE_256;
operationFinishHash.segmentLength = 112 - SHA2_DIGEST_LENGTH_BYTES_256;
operationFinishHash.message = message + SHA2_DIGEST_LENGTH_BYTES_256;
operationFinishHash.intermediateDigest = digest;
operationFinishHash.finalDigest = digest;
operationFinishHash.totalLength = 112;
testResult = SHA2_finishHash(handle, &operationFinishHash);
if (testResult != SHA2_STATUS_SUCCESS) {
while(1);
}
// The resultant digest should be:
// 0xcf, 0x5b, 0x16, 0xa7,
// 0x78, 0xaf, 0x83, 0x80,
// 0x03, 0x6c, 0xe5, 0x9e,
// 0x7b, 0x04, 0x92, 0x37,
// 0x0b, 0x24, 0x9b, 0x11,
// 0xe8, 0xf0, 0x7a, 0x51,
// 0xaf, 0xac, 0x45, 0x03,
// 0x7a, 0xfe, 0xe9, 0xd1
SHA2_close(handle);
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>

Go to the source code of this file.

Data Structures

struct  SHA2_OperationOneStep_
 Struct containing the parameters required to hash a message in one go. More...
 
struct  SHA2_OperationStartHash_
 Struct containing the parameters required to start hashing a message. More...
 
struct  SHA2_OperationProcessHash_
 Struct containing the parameters required to continue hashing a message. More...
 
struct  SHA2_OperationFinishlHash_
 Struct containing the parameters required to process the last blocks of a message and finalize the hash. More...
 
union  SHA2_Operation_
 Union containing pointers to all supported operation structs. More...
 
struct  SHA2_Config_
 SHA2 Global configuration. More...
 
struct  SHA2_Params_
 SHA2 Parameters. More...
 

Macros

#define SHA2_CMD_RESERVED   (32)
 
#define SHA2_STATUS_RESERVED   (-32)
 
#define SHA2_STATUS_SUCCESS   (0)
 Successful status code. More...
 
#define SHA2_STATUS_ERROR   (-1)
 Generic error status code. More...
 
#define SHA2_STATUS_UNDEFINEDCMD   (-2)
 An error status code returned by SHA2_control() for undefined command codes. More...
 
#define SHA2_STATUS_RESOURCE_UNAVAILABLE   (-3)
 An error status code returned if the hardware or software resource is currently unavailable. More...
 

Typedefs

typedef struct SHA2_Config_SHA2_Handle
 A handle that is returned from an SHA2_open() call. More...
 
typedef enum SHA2_ReturnBehavior_ SHA2_ReturnBehavior
 The way in which SHA2 function calls return after performing an operation. More...
 
typedef enum SHA2_HashSize_ SHA2_HashSize
 Enum for the hash digest sizes supported by the driver. More...
 
typedef enum SHA2_DigestLengthBytes_ SHA2_DigestLengthBytes
 Enum for the hash digest lengths in bytes supported by the driver. More...
 
typedef struct SHA2_OperationOneStep_ SHA2_OperationOneStepHash
 Struct containing the parameters required to hash a message in one go. More...
 
typedef struct SHA2_OperationStartHash_ SHA2_OperationStartHash
 Struct containing the parameters required to start hashing a message. More...
 
typedef struct SHA2_OperationProcessHash_ SHA2_OperationProcessHash
 Struct containing the parameters required to continue hashing a message. More...
 
typedef struct SHA2_OperationFinishlHash_ SHA2_OperationFinishHash
 Struct containing the parameters required to process the last blocks of a message and finalize the hash. More...
 
typedef union SHA2_Operation_ SHA2_Operation
 Union containing pointers to all supported operation structs. More...
 
typedef enum SHA2_OperationType_ SHA2_OperationType
 Enum for the operation types supported by the driver. More...
 
typedef struct SHA2_Config_ SHA2_Config
 SHA2 Global configuration. More...
 
typedef void(* SHA2_CallbackFxn) (SHA2_Handle handle, int_fast16_t returnStatus, SHA2_Operation operation, SHA2_OperationType operationType)
 The definition of a callback function used by the SHA2 driver when used in SHA2_RETURN_BEHAVIOR_CALLBACK. More...
 
typedef struct SHA2_Params_ SHA2_Params
 SHA2 Parameters. More...
 

Enumerations

enum  SHA2_ReturnBehavior_ { SHA2_RETURN_BEHAVIOR_CALLBACK = 1, SHA2_RETURN_BEHAVIOR_BLOCKING = 2, SHA2_RETURN_BEHAVIOR_POLLING = 4 }
 The way in which SHA2 function calls return after performing an operation. More...
 
enum  SHA2_HashSize_ { SHA2_HASH_SIZE_224 = 0, SHA2_HASH_SIZE_256 = 1, SHA2_HASH_SIZE_384 = 2, SHA2_HASH_SIZE_512 = 3 }
 Enum for the hash digest sizes supported by the driver. More...
 
enum  SHA2_DigestLengthBytes_ { SHA2_DIGEST_LENGTH_BYTES_224 = 28, SHA2_DIGEST_LENGTH_BYTES_256 = 32, SHA2_DIGEST_LENGTH_BYTES_384 = 48, SHA2_DIGEST_LENGTH_BYTES_512 = 64 }
 Enum for the hash digest lengths in bytes supported by the driver. More...
 
enum  SHA2_OperationType_ { SHA2_OPERATION_TYPE_START_HASH = 1, SHA2_OPERATION_TYPE_PROCESS_HASH = 2, SHA2_OPERATION_TYPE_FINISH_HASH = 3, SHA2_OPERATION_TYPE_ONE_STEP_HASH = 4 }
 Enum for the operation types supported by the driver. More...
 

Functions

void SHA2_init (void)
 This function initializes the SHA2 module. More...
 
void SHA2_Params_init (SHA2_Params *params)
 Function to initialize the SHA2_Params struct to its defaults. More...
 
SHA2_Handle SHA2_open (uint_least8_t index, SHA2_Params *params)
 This function opens a given SHA2 peripheral. More...
 
void SHA2_close (SHA2_Handle handle)
 Function to close a SHA2 peripheral specified by the SHA2 handle. More...
 
int_fast16_t SHA2_control (SHA2_Handle handle, uint32_t cmd, void *args)
 Function performs implementation specific features on a given SHA2_Handle. More...
 
void SHA2_OperationStartHash_init (SHA2_OperationStartHash *operation)
 Function to initialize a SHA2_OperationStartHash struct to its defaults. More...
 
void SHA2_OperationProcessHash_init (SHA2_OperationProcessHash *operation)
 Function to initialize a SHA2_OperationProcessHash struct to its defaults. More...
 
void SHA2_OperationFinishHash_init (SHA2_OperationFinishHash *operation)
 Function to initialize a SHA2_OperationFinishHash struct to its defaults. More...
 
void SHA2_OperationOneStepHash_init (SHA2_OperationOneStepHash *operation)
 Function to initialize a SHA2_OperationOneStepHash struct to its defaults. More...
 
int_fast16_t SHA2_startHash (SHA2_Handle handle, SHA2_OperationStartHash *operation)
 Sets up a SHA2 hash. More...
 
int_fast16_t SHA2_processHash (SHA2_Handle handle, SHA2_OperationProcessHash *operation)
 Performs the SHA2 hash on a part of the message. More...
 
int_fast16_t SHA2_finishHash (SHA2_Handle handle, SHA2_OperationFinishHash *operation)
 Completes final block(s) of hash and returns a final output hash value. More...
 
int_fast16_t SHA2_oneStepHash (SHA2_Handle handle, SHA2_OperationOneStepHash *operation)
 Hashes an input message. More...
 

Variables

const SHA2_Params SHA2_defaultParams
 Default SHA2_Params structure. More...
 

Typedef Documentation

§ SHA2_Handle

typedef struct SHA2_Config_* SHA2_Handle

A handle that is returned from an SHA2_open() call.

§ SHA2_ReturnBehavior

The way in which SHA2 function calls return after performing an operation.

Not all SHA2 operations exhibit the specified return behavor. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specfied return behavior is not implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.

SHA2 functions exhibiting the specified return behavior have restrictions on the context from which they may be called.

Task Hwi Swi
SHA2_RETURN_BEHAVIOR_CALLBACK X X X
SHA2_RETURN_BEHAVIOR_BLOCKING X
SHA2_RETURN_BEHAVIOR_POLLING X X X

§ SHA2_HashSize

Enum for the hash digest sizes supported by the driver.

§ SHA2_DigestLengthBytes

Enum for the hash digest lengths in bytes supported by the driver.

§ SHA2_OperationOneStepHash

Struct containing the parameters required to hash a message in one go.

§ SHA2_OperationStartHash

Struct containing the parameters required to start hashing a message.

§ SHA2_OperationProcessHash

Struct containing the parameters required to continue hashing a message.

§ SHA2_OperationFinishHash

Struct containing the parameters required to process the last blocks of a message and finalize the hash.

§ SHA2_Operation

Union containing pointers to all supported operation structs.

§ SHA2_OperationType

Enum for the operation types supported by the driver.

§ SHA2_Config

typedef struct SHA2_Config_ SHA2_Config

SHA2 Global configuration.

The SHA2_Config structure contains a set of pointers used to characterize the SHA2 driver implementation.

This structure needs to be defined before calling SHA2_init() and it must not be changed thereafter.

See also
SHA2_init()

§ SHA2_CallbackFxn

typedef void(* SHA2_CallbackFxn) (SHA2_Handle handle, int_fast16_t returnStatus, SHA2_Operation operation, SHA2_OperationType operationType)

The definition of a callback function used by the SHA2 driver when used in SHA2_RETURN_BEHAVIOR_CALLBACK.

Parameters
handleHandle of the client that started the SHA2 operation.
returnStatusThe result of the ECDH operation. May contain an error code if the result is the point at infinity for example.
operationA union of pointers to operation structs. Only one type of pointer is valid per call to the callback function. Which type is currently valid is determined by /c operationType. The union allows easier access to the struct's fields without the need to typecase the result.
operationTypeThis parameter determined which operation the callback refers to and which type to access through /c operation.

§ SHA2_Params

typedef struct SHA2_Params_ SHA2_Params

SHA2 Parameters.

SHA2 Parameters are used to with the SHA2_open() call. Default values for these parameters are set using SHA2_Params_init().

See also
SHA2_Params_init()

Enumeration Type Documentation

§ SHA2_ReturnBehavior_

The way in which SHA2 function calls return after performing an operation.

Not all SHA2 operations exhibit the specified return behavor. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specfied return behavior is not implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.

SHA2 functions exhibiting the specified return behavior have restrictions on the context from which they may be called.

Task Hwi Swi
SHA2_RETURN_BEHAVIOR_CALLBACK X X X
SHA2_RETURN_BEHAVIOR_BLOCKING X
SHA2_RETURN_BEHAVIOR_POLLING X X X
Enumerator
SHA2_RETURN_BEHAVIOR_CALLBACK 

The function call will return immediately while the SHA2 operation goes on in the background. The registered callback function is called after the operation completes. The context the callback function is called (task, HWI, SWI) is implementation-dependent.

SHA2_RETURN_BEHAVIOR_BLOCKING 

The function call will block while SHA2 operation goes on in the background. SHA2 operation results are available after the function returns.

SHA2_RETURN_BEHAVIOR_POLLING 

The function call will continuously poll a flag while SHA2 operation goes on in the background. SHA2 operation results are available after the function returns.

§ SHA2_HashSize_

Enum for the hash digest sizes supported by the driver.

Enumerator
SHA2_HASH_SIZE_224 
SHA2_HASH_SIZE_256 
SHA2_HASH_SIZE_384 
SHA2_HASH_SIZE_512 

§ SHA2_DigestLengthBytes_

Enum for the hash digest lengths in bytes supported by the driver.

Enumerator
SHA2_DIGEST_LENGTH_BYTES_224 
SHA2_DIGEST_LENGTH_BYTES_256 
SHA2_DIGEST_LENGTH_BYTES_384 
SHA2_DIGEST_LENGTH_BYTES_512 

§ SHA2_OperationType_

Enum for the operation types supported by the driver.

Enumerator
SHA2_OPERATION_TYPE_START_HASH 
SHA2_OPERATION_TYPE_PROCESS_HASH 
SHA2_OPERATION_TYPE_FINISH_HASH 
SHA2_OPERATION_TYPE_ONE_STEP_HASH 

Function Documentation

§ SHA2_init()

void SHA2_init ( void  )

This function initializes the SHA2 module.

Precondition
The SHA2_config structure must exist and be persistent before this function can be called. This function must also be called before any other SHA2 driver APIs. This function call does not modify any peripheral registers.

§ SHA2_Params_init()

void SHA2_Params_init ( SHA2_Params params)

Function to initialize the SHA2_Params struct to its defaults.

Parameters
paramsAn pointer to SHA2_Params structure for initialization

Defaults values are: returnBehavior = SHA2_RETURN_BEHAVIOR_BLOCKING callbackFxn = NULL timeout = SemaphoreP_WAIT_FOREVER custom = NULL

§ SHA2_open()

SHA2_Handle SHA2_open ( uint_least8_t  index,
SHA2_Params params 
)

This function opens a given SHA2 peripheral.

Precondition
SHA2 controller has been initialized using SHA2_init()
Parameters
indexLogical peripheral number for the SHA2 indexed into the SHA2_config table
paramsPointer to an parameter block, if NULL it will use default values.
Returns
A SHA2_Handle on success or a NULL on an error or if it has been opened already.
See also
SHA2_init()
SHA2_close()

§ SHA2_close()

void SHA2_close ( SHA2_Handle  handle)

Function to close a SHA2 peripheral specified by the SHA2 handle.

Precondition
SHA2_open() has to be called first.
Parameters
handleA SHA2 handle returned from SHA2_open()
See also
SHA2_open()

§ SHA2_control()

int_fast16_t SHA2_control ( SHA2_Handle  handle,
uint32_t  cmd,
void *  args 
)

Function performs implementation specific features on a given SHA2_Handle.

Commands for SHA2_control can originate from SHA2.h or from implementation specific SHA2*.h (SHA2CC26XX.h, SHA2MSP432.h, etc.. ) files. While commands from SHA2.h are API portable across driver implementations, not all implementations may support all these commands. Conversely, commands from driver implementation specific SHA2*.h files add unique driver capabilities but are not API portable across all SHA2 driver implementations.

Commands supported by SHA2.h follow an SHA2_CMD_<cmd> naming convention.
Commands supported by SHA2*.h follow an SHA2*_CMD_<cmd> naming convention.
Each control command defines arg differently. The types of arg are documented with each command.

See SHA2_control command codes for command codes.

See SHA2_control return status codes for status codes.

Precondition
SHA2_open() has to be called first.
Parameters
handleA SHA2 handle returned from SHA2_open()
cmdSHA2.h or SHA2*.h commands.
argsAn optional R/W (read/write) command argument accompanied with cmd
Returns
Implementation specific return codes. Negative values indicate unsuccessful operations.
See also
SHA2_open()

§ SHA2_OperationStartHash_init()

void SHA2_OperationStartHash_init ( SHA2_OperationStartHash operation)

Function to initialize a SHA2_OperationStartHash struct to its defaults.

Parameters
operationA pointer to SHA2_OperationStartHash structure for initialization

Defaults values are all zeros.

§ SHA2_OperationProcessHash_init()

void SHA2_OperationProcessHash_init ( SHA2_OperationProcessHash operation)

Function to initialize a SHA2_OperationProcessHash struct to its defaults.

Parameters
operationA pointer to SHA2_OperationProcessHash structure for initialization

Defaults values are all zeros.

§ SHA2_OperationFinishHash_init()

void SHA2_OperationFinishHash_init ( SHA2_OperationFinishHash operation)

Function to initialize a SHA2_OperationFinishHash struct to its defaults.

Parameters
operationA pointer to SHA2_OperationFinishHash structure for initialization

Defaults values are all zeros.

§ SHA2_OperationOneStepHash_init()

void SHA2_OperationOneStepHash_init ( SHA2_OperationOneStepHash operation)

Function to initialize a SHA2_OperationOneStepHash struct to its defaults.

Parameters
operationA pointer to SHA2_OperationOneStepHash structure for initialization

Defaults values are all zeros.

§ SHA2_startHash()

int_fast16_t SHA2_startHash ( SHA2_Handle  handle,
SHA2_OperationStartHash operation 
)

Sets up a SHA2 hash.

Precondition
SHA2_open() has to be called first.
Parameters
handleA SHA2 handle returned from SHA2_open()
operationA pointer to a struct containing the requisite parameters to execute the function.
See also
SHA2_open()
SHA2_processHash()
SHA2_finishHash()

§ SHA2_processHash()

int_fast16_t SHA2_processHash ( SHA2_Handle  handle,
SHA2_OperationProcessHash operation 
)

Performs the SHA2 hash on a part of the message.

SHA2_processHash() should be used when only part of a message is available for hashing.

Precondition
SHA2_startHash() must be called before a SHA2_processHash may be called.
Note
SHA2_processHash() should NOT be used for the final block of the hash. If the entire message is available for hashing, SHA2_processHash() should not be called, and instead entire message may be hashed with SHA2_finishHash().
Parameters
handleA SHA2 handle returned from SHA2_open()
operationA pointer to a struct containing the requisite parameters to execute the function.
See also
SHA2_startHash()
SHA2_finishHash()

§ SHA2_finishHash()

int_fast16_t SHA2_finishHash ( SHA2_Handle  handle,
SHA2_OperationFinishHash operation 
)

Completes final block(s) of hash and returns a final output hash value.

SHA2_finishHash() must be used to digest the final block of the hash, and may also be used to digest some or all preceding blocks of the message.

Precondition
SHA2_startHash() must be called before a SHA2_finishHash() may be called; SHA2_processHash() may optionally be called before SHA2_finishHash().
Parameters
handleA SHA2 handle returned from SHA2_open().
operationA pointer to a struct containing the requisite parameters to execute the function.
See also
SHA2_startHash()
SHA2_processHash()

§ SHA2_oneStepHash()

int_fast16_t SHA2_oneStepHash ( SHA2_Handle  handle,
SHA2_OperationOneStepHash operation 
)

Hashes an input message.

SHA2_oneStepHash() hashes a message stored contiguously. Use this function if you have access to the entire message when starting to hash.

Precondition
SHA2_open() must be called prior.
Parameters
handleA SHA2 handle returned from SHA2_open().
operationA pointer to a struct containing the requisite parameters to execute the function.

Variable Documentation

§ SHA2_defaultParams

const SHA2_Params SHA2_defaultParams

Default SHA2_Params structure.

See also
SHA2_Params_init()
Copyright 2017, Texas Instruments Incorporated