![]() |
0.01.00
|
This file includes definitions for manipulating IPv6 routing tables. More...
#include "openthread-core-config.h"#include <openthread/types.h>#include "common/locator.hpp"#include "common/message.hpp"#include "net/ip6_address.hpp"#include "net/ip6_routes.hpp"Go to the source code of this file.
Classes | |
| struct | ot::Ip6::Route |
| This structure represents an IPv6 route. More... | |
| class | ot::Ip6::Routes |
| This class implements IPv6 route management. More... | |
Namespaces | |
| ot::Ip6 | |
| This namespace includes definitions for IPv6 networking. | |
This file includes definitions for manipulating IPv6 routing tables.