![]() |
0.01.00
|
This is the complete list of members for ot::ExtendedTlv, including all inherited members.
| Get(const Message &aMessage, uint8_t aType, uint16_t aMaxLength, Tlv &aTlv) | ot::Tlv | static |
| GetLength(void) const | ot::ExtendedTlv | inline |
| GetNext(void) | ot::Tlv | inline |
| GetNext(void) const | ot::Tlv | inline |
| GetOffset(const Message &aMessage, uint8_t aType, uint16_t &aOffset) | ot::Tlv | static |
| GetSize(void) const | ot::Tlv | inline |
| GetType(void) const | ot::Tlv | inline |
| GetValue(void) | ot::Tlv | inline |
| GetValue(void) const | ot::Tlv | inline |
| GetValueOffset(const Message &aMesasge, uint8_t aType, uint16_t &aOffset, uint16_t &aLength) | ot::Tlv | static |
| kExtendedLength enum value | ot::Tlv | protected |
| SetLength(uint16_t aLength) | ot::ExtendedTlv | inline |
| ot::Tlv::SetLength(uint8_t aLength) | ot::Tlv | inline |
| SetType(uint8_t aType) | ot::Tlv | inline |
| Tlv(void) | ot::Tlv | inline |