![]() |
0.01.00
|
This structure represents a UDP socket. More...
#include <include/openthread/udp.h>
Public Attributes | |
| otSockAddr | mSockName |
| The local IPv6 socket address. | |
| otSockAddr | mPeerName |
| The peer IPv6 socket address. | |
| otUdpReceive | mHandler |
| A function pointer to the application callback. | |
| void * | mContext |
| A pointer to application-specific context. | |
| void * | mTransport |
| A pointer to the transport object (internal use only). | |
| struct otUdpSocket * | mNext |
| A pointer to the next UDP socket (internal use only). | |
This structure represents a UDP socket.