§ TmfProxy()
This constructor initializes the TMF proxy.
- Parameters
-
| [in] | aMeshLocal16 | A reference to the Mesh Local Routing Locator. |
| [in] | aCoap | A reference to the Management CoAP Service. |
§ IsEnabled()
| bool ot::TmfProxy::IsEnabled |
( |
void |
| ) |
const |
This method indicates whether or not the TMF proxy service is enabled.
- Return values
-
| TRUE | If the service is enabled. |
| FALSE | If the service is disabled. |
§ Send()
| otError ot::TmfProxy::Send |
( |
Message & |
aMessage, |
|
|
uint16_t |
aLocator, |
|
|
uint16_t |
aPort |
|
) |
| |
This method sends the message into the thread network.
- Parameters
-
| [in] | aMessage | A reference to the message to send. |
| [in] | aLocator | The destination's RLOC16 or ALOC16. |
| [in] | aPort | The destination port. |
- Return values
-
| OT_ERROR_NONE | Successfully send the message. |
| OT_ERROR_INVALID_STATE | Border agent proxy is not started. |
- Warning
- No matter the call success or fail, the message is freed.
§ Start()
This method enables the TMF proxy service.
- Return values
-
| OT_ERROR_NONE | Successfully started the service. |
| OT_ERROR_ALREADY | The service already started. |
§ Stop()
| otError ot::TmfProxy::Stop |
( |
void |
| ) |
|
This method disables the TMF proxy service.
- Return values
-
| OT_ERROR_NONE | Successfully stopped the TMF proxy service. |
| OT_ERROR_ALREADY | The service already stopped. |
The documentation for this class was generated from the following file: