![]() |
0.01.00
|
This file includes definitions for the Commissioner role. More...
#include "openthread-core-config.h"#include <openthread/commissioner.h>#include "coap/coap.hpp"#include "coap/coap_secure.hpp"#include "common/locator.hpp"#include "common/timer.hpp"#include "mac/mac_frame.hpp"#include "meshcop/announce_begin_client.hpp"#include "meshcop/dtls.hpp"#include "meshcop/energy_scan_client.hpp"#include "meshcop/panid_query_client.hpp"#include "net/udp6.hpp"#include "thread/mle.hpp"Go to the source code of this file.
Classes | |
| class | ot::MeshCoP::Commissioner |
This file includes definitions for the Commissioner role.