![]() |
0.01.00
|
This structure represents the message buffer information. More...
#include <include/openthread/types.h>
Public Attributes | |
| uint16_t | mTotalBuffers |
| The number of buffers in the pool. | |
| uint16_t | mFreeBuffers |
| The number of free message buffers. | |
| uint16_t | m6loSendMessages |
| The number of messages in the 6lo send queue. | |
| uint16_t | m6loSendBuffers |
| The number of buffers in the 6lo send queue. | |
| uint16_t | m6loReassemblyMessages |
| The number of messages in the 6LoWPAN reassembly queue. | |
| uint16_t | m6loReassemblyBuffers |
| The number of buffers in the 6LoWPAN reassembly queue. | |
| uint16_t | mIp6Messages |
| The number of messages in the IPv6 send queue. | |
| uint16_t | mIp6Buffers |
| The number of buffers in the IPv6 send queue. | |
| uint16_t | mMplMessages |
| The number of messages in the MPL send queue. | |
| uint16_t | mMplBuffers |
| The number of buffers in the MPL send queue. | |
| uint16_t | mMleMessages |
| The number of messages in the MLE send queue. | |
| uint16_t | mMleBuffers |
| The number of buffers in the MLE send queue. | |
| uint16_t | mArpMessages |
| The number of messages in the ARP send queue. | |
| uint16_t | mArpBuffers |
| The number of buffers in the ARP send queue. | |
| uint16_t | mCoapMessages |
| The number of messages in the CoAP send queue. | |
| uint16_t | mCoapBuffers |
| The number of buffers in the CoAP send queue. | |
| uint16_t | mCoapSecureMessages |
| The number of messages in the CoAP secure send queue. | |
| uint16_t | mCoapSecureBuffers |
| The number of buffers in the CoAP secure send queue. | |
| uint16_t | mApplicationCoapMessages |
| The number of messages in the application CoAP send queue. | |
| uint16_t | mApplicationCoapBuffers |
| The number of buffers in the application CoAP send queue. | |
This structure represents the message buffer information.