![]() |
0.01.00
|
This file is a wrapper for the standard "string.h" file The purpose is add any missing function prototypes not provided by a specific compiler. More...
Go to the source code of this file.
Macros | |
| #define | __bool_true_false_are_defined 1 |
| #define | false 0 |
| #define | true 1 |
Typedefs | |
| typedef _Bool | bool |
This file is a wrapper for the standard "string.h" file The purpose is add any missing function prototypes not provided by a specific compiler.