![]() |
0.01.00
|
This struct represents a received IEEE 802.15.4 Beacon. More...
#include <include/openthread/types.h>
Public Attributes | |
| otExtAddress | mExtAddress |
| IEEE 802.15.4 Extended Address. | |
| otNetworkName | mNetworkName |
| Thread Network Name. | |
| otExtendedPanId | mExtendedPanId |
| Thread Extended PAN ID. | |
| otSteeringData | mSteeringData |
| Steering Data. | |
| uint16_t | mPanId |
| IEEE 802.15.4 PAN ID. | |
| uint16_t | mJoinerUdpPort |
| Joiner UDP Port. | |
| uint8_t | mChannel |
| IEEE 802.15.4 Channel. | |
| int8_t | mRssi |
| RSSI (dBm) | |
| uint8_t | mLqi |
| LQI. | |
| unsigned int | mVersion: 4 |
| Version. | |
| bool | mIsNative: 1 |
| Native Commissioner flag. | |
| bool | mIsJoinable: 1 |
| Joining Permitted flag. | |
This struct represents a received IEEE 802.15.4 Beacon.