#include <stdbool.h>#include <stdint.h>#include "../inc/hw_types.h"#include "../inc/hw_trng.h"#include "../inc/hw_memmap.h"#include "../inc/hw_ints.h"#include "debug.h"#include "interrupt.h"#include "cpu.h"Macros | |
| #define | TRNG_NUMBER_READY 0x00000001 |
| #define | TRNG_FRO_SHUTDOWN 0x00000002 |
| #define | TRNG_NEED_CLOCK 0x80000000 |
| #define | TRNG_HI_WORD 0x00000001 |
| #define | TRNG_LOW_WORD 0x00000002 |
Functions | |
| void | TRNGConfigure (uint32_t ui32MinSamplesPerCycle, uint32_t ui32MaxSamplesPerCycle, uint32_t ui32ClocksPerSample) |
| Configure the true random number generator. More... | |
| static void | TRNGEnable (void) |
| Enable the TRNG. More... | |
| static void | TRNGDisable (void) |
| Disable the TRNG module. More... | |
| uint32_t | TRNGNumberGet (uint32_t ui32Word) |
| Get a random number from the generator. More... | |
| static uint32_t | TRNGStatusGet (void) |
| Get the status of the TRNG. More... | |
| static void | TRNGReset (void) |
| Reset the TRNG. More... | |
| static void | TRNGIntEnable (uint32_t ui32IntFlags) |
| Enables individual TRNG interrupt sources. More... | |
| static void | TRNGIntDisable (uint32_t ui32IntFlags) |
| Disables individual TRNG interrupt sources. More... | |
| static uint32_t | TRNGIntStatus (bool bMasked) |
| Gets the current interrupt status of the TRNG module. More... | |
| static void | TRNGIntClear (uint32_t ui32IntFlags) |
| Clears TRNG interrupt sources. More... | |
| static void | TRNGIntRegister (void(*pfnHandler)(void)) |
| Registers an interrupt handler for a TRNG interrupt in the dynamic interrupt table. More... | |
| static void | TRNGIntUnregister (void) |
| Unregisters an interrupt handler for a TRNG interrupt in the dynamic interrupt table. More... | |