|
| static uint32_t | TimerIntNumberGet (uint32_t ui32Base) |
| | Gets the timer interrupt number. More...
|
| |
| void | TimerConfigure (uint32_t ui32Base, uint32_t ui32Config) |
| | Configures the timer(s). More...
|
| |
| void | TimerLevelControl (uint32_t ui32Base, uint32_t ui32Timer, bool bInvert) |
| | Controls the output level. More...
|
| |
| void | TimerStallControl (uint32_t ui32Base, uint32_t ui32Timer, bool bStall) |
| | Controls the stall handling. More...
|
| |
| void | TimerWaitOnTriggerControl (uint32_t ui32Base, uint32_t ui32Timer, bool bWait) |
| | Controls the wait on trigger handling. More...
|
| |
| void | TimerIntRegister (uint32_t ui32Base, uint32_t ui32Timer, void(*pfnHandler)(void)) |
| | Registers an interrupt handler for the timer interrupt in the dynamic interrupt table. More...
|
| |
| void | TimerIntUnregister (uint32_t ui32Base, uint32_t ui32Timer) |
| | Unregisters an interrupt handler for the timer interrupt in the dynamic interrupt table. More...
|
| |
| void | TimerMatchUpdateMode (uint32_t ui32Base, uint32_t ui32Timer, uint32_t ui32Mode) |
| | Sets the Match Register Update mode. More...
|
| |
| void | TimerIntervalLoadMode (uint32_t ui32Base, uint32_t ui32Timer, uint32_t ui32Mode) |
| | Sets the Interval Load mode. More...
|
| |