#include "../inc/hw_types.h"#include "../inc/hw_ccfg.h"#include "../inc/hw_ioc.h"#include "aon_batmon.h"#include "flash.h"#include "gpio.h"#include "setup_rom.h"#include "sys_ctrl.h"Functions | |
| void | SysCtrlIdle (uint32_t vimsPdMode) |
| Force the system into idle mode. More... | |
| void | SysCtrlShutdownWithAbort (void) |
| Try to enter shutdown but abort if wakeup event happened before shutdown. More... | |
| void | SysCtrlShutdown (void) |
| Enable shutdown of the device. More... | |
| void | SysCtrlStandby (bool retainCache, uint32_t vimsPdMode, uint32_t rechargeMode) |
| Force the system into standby mode. More... | |
| void | SysCtrlSetRechargeBeforePowerDown (uint32_t xoscPowerMode) |
| Set Recharge values before entering Power Down. More... | |
| void | SysCtrlAdjustRechargeAfterPowerDown (uint32_t vddrRechargeMargin) |
| Adjust Recharge calculations to be used next. More... | |
| void | SysCtrl_DCDC_VoltageConditionalControl (void) |
| Turns DCDC on or off depending of what is considered to be optimal usage. More... | |
| uint32_t | SysCtrlResetSourceGet (void) |
| Returns the reset source (including "wakeup from shutdown"). More... | |