|
| uint32_t | PKAGetOpsStatus (void) |
| | Gets the PKA operation status. More...
|
| |
| uint32_t | PKABigNumModStart (const uint8_t *bigNum, uint32_t bigNumLength, const uint8_t *modulus, uint32_t modulusLength, uint32_t *resultPKAMemAddr) |
| | Starts a big number modulus operation. More...
|
| |
| uint32_t | PKABigNumModGetResult (uint8_t *resultBuf, uint32_t length, uint32_t resultPKAMemAddr) |
| | Gets the result of the big number modulus operation. More...
|
| |
| uint32_t | PKABigNumCmpStart (const uint8_t *bigNum1, const uint8_t *bigNum2, uint32_t length) |
| | Starts the comparison of two big numbers. More...
|
| |
| uint32_t | PKABigNumCmpGetResult (void) |
| | Gets the result of the comparison operation of two big numbers. More...
|
| |
| uint32_t | PKABigNumInvModStart (const uint8_t *bigNum, uint32_t bigNumLength, const uint8_t *modulus, uint32_t modulusLength, uint32_t *resultPKAMemAddr) |
| | Starts a big number inverse modulo operation. More...
|
| |
| uint32_t | PKABigNumInvModGetResult (uint8_t *resultBuf, uint32_t length, uint32_t resultPKAMemAddr) |
| | Gets the result of the big number inverse modulo operation. More...
|
| |
| uint32_t | PKABigNumMultiplyStart (const uint8_t *multiplicand, uint32_t multiplicandLength, const uint8_t *multiplier, uint32_t multiplierLength, uint32_t *resultPKAMemAddr) |
| | Starts the multiplication of two big numbers. More...
|
| |
| uint32_t | PKABigNumMultGetResult (uint8_t *resultBuf, uint32_t *resultLength, uint32_t resultPKAMemAddr) |
| | Gets the result of the big number multiplication. More...
|
| |
| uint32_t | PKABigNumAddStart (const uint8_t *bigNum1, uint32_t bigNum1Length, const uint8_t *bigNum2, uint32_t bigNum2Length, uint32_t *resultPKAMemAddr) |
| | Starts the addition of two big numbers. More...
|
| |
| uint32_t | PKABigNumAddGetResult (uint8_t *resultBuf, uint32_t *resultLength, uint32_t resultPKAMemAddr) |
| | Gets the result of the addition operation on two big numbers. More...
|
| |
| uint32_t | PKABigNumSubStart (const uint8_t *minuend, uint32_t minuendLength, const uint8_t *subtrahend, uint32_t subtrahendLength, uint32_t *resultPKAMemAddr) |
| | Starts the subtration of one big number from another. More...
|
| |
| uint32_t | PKABigNumSubGetResult (uint8_t *resultBuf, uint32_t *resultLength, uint32_t resultPKAMemAddr) |
| | Gets the result of the subtration operation on two big numbers. More...
|
| |
| uint32_t | PKAEccMultiplyStart (const uint8_t *scalar, const uint8_t *curvePointX, const uint8_t *curvePointY, const uint8_t *prime, const uint8_t *a, const uint8_t *b, uint32_t length, uint32_t *resultPKAMemAddr) |
| | Starts ECC multiplication. More...
|
| |
| uint32_t | PKAEccMultiplyGetResult (uint8_t *curvePointX, uint8_t *curvePointY, uint32_t resultPKAMemAddr, uint32_t length) |
| | Gets the result of ECC multiplication. More...
|
| |
| uint32_t | PKAEccAddStart (const uint8_t *curvePoint1X, const uint8_t *curvePoint1Y, const uint8_t *curvePoint2X, const uint8_t *curvePoint2Y, const uint8_t *prime, const uint8_t *a, uint32_t length, uint32_t *resultPKAMemAddr) |
| | Starts the ECC addition. More...
|
| |
| uint32_t | PKAEccAddGetResult (uint8_t *curvePointX, uint8_t *curvePointY, uint32_t resultPKAMemAddr, uint32_t length) |
| | Gets the result of the ECC addition. More...
|
| |