Changes the AUX operational mode to the requested target mode.
This function controls the change of the AUX operational mode. The function controls the change of the current operational mode to the operational mode target by adhering to rules specified by HW.
- Parameters
-
| targetOpMode | AUX operational mode:
|
- Returns
- None
Referenced by TrimAfterColdResetWakeupFromShutDown().
69 uint32_t currentOpMode;
70 uint32_t currentOrder;
83 if (currentOpMode != targetOpMode)
96 }
while ( currentOpMode != targetOpMode );
static const uint8_t g_Order_to_OpMode[4]
Definition: aux_sysif.c:59
#define ASSERT(expr)
Definition: debug.h:73
#define MCU_RAM_RET_FULL
Definition: aon_pmctl.h:80
static const uint8_t g_OpMode_to_order[4]
Definition: aux_sysif.c:58