|
| uint32_t | CRYPTOAesLoadKey (uint32_t *pui32AesKey, uint32_t ui32KeyLocation) |
| | Write the key into the Key Ram. More...
|
| |
| uint32_t | CRYPTOAesCbc (uint32_t *pui32MsgIn, uint32_t *pui32MsgOut, uint32_t ui32MsgLength, uint32_t *pui32Nonce, uint32_t ui32KeyLocation, bool bEncrypt, bool bIntEnable) |
| | Start an AES-CBC operation (encryption or decryption). More...
|
| |
| uint32_t | CRYPTOAesCbcStatus (void) |
| | Check the result of an AES CBC operation. More...
|
| |
| uint32_t | CRYPTOAesEcb (uint32_t *pui32MsgIn, uint32_t *pui32MsgOut, uint32_t ui32KeyLocation, bool bEncrypt, bool bIntEnable) |
| | Start an AES-ECB operation (encryption or decryption). More...
|
| |
| uint32_t | CRYPTOAesEcbStatus (void) |
| | Check the result of an AES ECB operation. More...
|
| |
| static void | CRYPTOAesEcbFinish (void) |
| | Finish the encryption operation by resetting the operation mode. More...
|
| |
| static void | CRYPTOAesCbcFinish (void) |
| | Finish the encryption operation by resetting the operation mode. More...
|
| |
| uint32_t | CRYPTOCcmAuthEncrypt (bool bEncrypt, uint32_t ui32AuthLength, uint32_t *pui32Nonce, uint32_t *pui32PlainText, uint32_t ui32PlainTextLength, uint32_t *pui32Header, uint32_t ui32HeaderLength, uint32_t ui32KeyLocation, uint32_t ui32FieldLength, bool bIntEnable) |
| | Start CCM operation. More...
|
| |
| uint32_t | CRYPTOCcmAuthEncryptStatus (void) |
| | Check the result of an AES CCM operation. More...
|
| |
| uint32_t | CRYPTOCcmAuthEncryptResultGet (uint32_t ui32TagLength, uint32_t *pui32CcmTag) |
| | Get the result of an AES CCM operation. More...
|
| |
| uint32_t | CRYPTOCcmInvAuthDecrypt (bool bDecrypt, uint32_t ui32AuthLength, uint32_t *pui32Nonce, uint32_t *pui32CipherText, uint32_t ui32CipherTextLength, uint32_t *pui32Header, uint32_t ui32HeaderLength, uint32_t ui32KeyLocation, uint32_t ui32FieldLength, bool bIntEnable) |
| | Start a CCM Decryption and Inverse Authentication operation. More...
|
| |
| uint32_t | CRYPTOCcmInvAuthDecryptStatus (void) |
| | Checks CCM decrypt and Inverse Authentication result. More...
|
| |
| uint32_t | CRYPTOCcmInvAuthDecryptResultGet (uint32_t ui32AuthLength, uint32_t *pui32CipherText, uint32_t ui32CipherTextLength, uint32_t *pui32CcmTag) |
| | Get the result of the CCM operation. More...
|
| |
| static uint32_t | CRYPTODmaStatus (void) |
| | Get the current status of the Crypto DMA controller. More...
|
| |
| void | CRYPTODmaEnable (uint32_t ui32Channels) |
| | Enable Crypto DMA operation. More...
|
| |
| void | CRYPTODmaDisable (uint32_t ui32Channels) |
| | Disable Crypto DMA operation. More...
|
| |
| static void | CRYPTOIntEnable (uint32_t ui32IntFlags) |
| | Enables individual Crypto interrupt sources. More...
|
| |
| static void | CRYPTOIntDisable (uint32_t ui32IntFlags) |
| | Disables individual CRYPTO interrupt sources. More...
|
| |
| static uint32_t | CRYPTOIntStatus (bool bMasked) |
| | Gets the current interrupt status. More...
|
| |
| static void | CRYPTOIntClear (uint32_t ui32IntFlags) |
| | Clears Crypto interrupt sources. More...
|
| |
| static void | CRYPTOIntRegister (void(*pfnHandler)(void)) |
| | Registers an interrupt handler for a Crypto interrupt in the dynamic interrupt table. More...
|
| |
| static void | CRYPTOIntUnregister (void) |
| | Unregisters an interrupt handler for a Crypto interrupt in the dynamic interrupt table. More...
|
| |