![]() |
![]() |
Display driver for printf-like output.
============================================================================
The header file should be included in an application as follows:
Below is an example configuration to use the HOST display.
For TIRTOS based applications, the Display_HOST interface is only callable from Task context. The Display_HOST interface is callable from any context for FreeRTOS based applications.
#include <ti/display/Display.h>
Go to the source code of this file.
Data Structures | |
struct | DisplayHost_HWAttrs |
DisplayHost Attributes. More... | |
struct | DisplayHost_Object |
DisplayHost Object. More... | |
Typedefs | |
typedef struct DisplayHost_HWAttrs | DisplayHost_HWAttrs |
DisplayHost Attributes. More... | |