TI BLE5-Stack API Documentation  1.01.01.00
Data Fields
hciEvt_CmdComplete_t Struct Reference

Command Complete Event. More...

Data Fields

uint16 cmdOpcode
 command opcode
 
osal_event_hdr_t hdr
 osal event header
 
uint8 numHciCmdPkt
 number of HCI Command Packet
 
uint8 * pReturnParam
 pointer to the return parameter
 

Detailed Description

Command Complete Event.


The documentation for this struct was generated from the following file:
Copyright 2018, Texas Instruments Incorporated