TI BLE5-Stack API Documentation  1.01.01.00
Data Fields
gattMsgEvent_t Struct Reference

GATT GATT_MSG_EVENT message format. More...

Data Fields

uint16 connHandle
 Connection message was received on.
 
osal_event_hdr_t hdr
 GATT_MSG_EVENT and status.
 
uint8 method
 Type of message.
 
gattMsg_t msg
 Attribute protocol/profile message.
 

Detailed Description

GATT GATT_MSG_EVENT message format.

This message is used to forward an incoming attribute protocol/profile message up to upper layer application.


The documentation for this struct was generated from the following file:
Copyright 2018, Texas Instruments Incorporated