TI BLE5-Stack API Documentation  1.01.01.00
Data Fields
attFindByTypeValueReq_t Struct Reference

Find By Type Value Request format. More...

Data Fields

uint16 endHandle
 Last requested handle number.
 
uint16 len
 Length of value.
 
uint8 * pValue
 Attribute value to find (0 to ATT_MTU_SIZE-7)
 
uint16 startHandle
 First requested handle number (must be first field)
 
attAttrBtType_t type
 2-octet UUID to find
 

Detailed Description

Find By Type Value Request format.

for method ATT_FIND_BY_TYPE_VALUE_REQ


The documentation for this struct was generated from the following file:
Copyright 2018, Texas Instruments Incorporated