TI BLE5-Stack API Documentation  1.01.01.00
Modules | Files | Data Structures | Macros | Typedefs | Enumerations | Functions
OAD BLE Profile

BLE Profile implementation of the TI over the air download solution. This file is responsible for processing data from the BLE-Stack, passing this data to the application, and processing queued OAD events as well as the OAD state machine. More...

Modules

 OAD Events
 
 OAD Extended Control Command op codes
 
 OAD Service Indexes
 
 OAD Service UUIDs
 
 OAD return status codes
 

Files

file  oad.h
 This file contains OAD Profile header file.
 

Data Structures

struct  blockReqPld_t
 
struct  blockSizeRspPld_t
 
struct  deviceTypeRspPld_t
 
struct  extImgEnableReq_t
 
struct  genericExtCtrlRsp_t
 
struct  imageInfo_t
 
struct  imageInfoRspPld_t
 
struct  imgIdentifyPld_t
 
struct  oadTargetCBs_t
 
struct  oadTargetWrite_t
 
struct  profileVerRsp_t
 
struct  swVersionPld_t
 

Macros

#define EXT_CTRL_OP_CODE(pData)   (pData[0])
 
#define OAD_ATT_OVERHEAD   3
 
#define OAD_BLK_NUM_HDR_SZ   4
 
#define OAD_CCCD_CNT   OAD_CHAR_CNT
 
#define OAD_CHAR_CNT   3
 
#define OAD_DEFAULT_BLOCK_SIZE   20
 
#define OAD_DEFAULT_INACTIVITY_TIME   10000
 
#define OAD_EFL_MAX_META   4
 
#define OAD_EXT_CTRL_CMD_NOT_SUPPORTED   0xFF
 
#define OAD_IMAGE_ID_RSP_LEN   0x01
 
#define OAD_IMG_ID_RETRIES   3
 
#define OAD_IMG_INFO_ONCHIP   0x01
 
#define OAD_IMG_PG_INVALID   0xFF
 
#define OAD_MAX_BLOCK_SIZE   244
 
#define OAD_MIN_INACTIVITY_TIME   4000
 
#define OAD_WRITE_PERMIT   GATT_PERMIT_WRITE
 

Typedefs

typedef void(* oadWriteCB_t) (uint8_t event, uint16_t arg)
 

Enumerations

enum  oadEvent_e {
  OAD_WRITE_IDENTIFY_REQ, OAD_WRITE_BLOCK_REQ, OAD_IMAGE_COMPLETE, OAD_EXT_CTRL_WRITE_CMD,
  OAD_TIMEOUT
}
 
enum  oadState_e {
  OAD_IDLE, OAD_VALIDATE_IMG, OAD_CONFIG, OAD_DOWNLOAD,
  OAD_CHECK_DL, OAD_COMPLETE
}
 

Functions

void OAD_cancel (void)
 
void OAD_close (void)
 
uint16_t OAD_getactiveCxnHandle ()
 
uint16_t OAD_getBlockSize (void)
 
bool OAD_getSWVersion (uint8_t *swVer, uint8_t len)
 
bool OAD_isUsrAppValid (void)
 
uint8_t OAD_open (uint32_t oadTimeout)
 
uint8_t OAD_processQueue (void)
 
void OAD_register (oadTargetCBs_t *pfnOadCBs)
 
uint8_t OAD_setBlockSize (uint16_t mtuSize)
 
uint8_t oadCreateFactoryImageBackup (void)
 

Detailed Description

BLE Profile implementation of the TI over the air download solution. This file is responsible for processing data from the BLE-Stack, passing this data to the application, and processing queued OAD events as well as the OAD state machine.

============================================================================

Header Include

The OAD Profile header should be included in an OAD enabled application as follows:

Overview

This module is intended to handle OAD related functionality for the application. At a high level it is responsible for receiving and parsing OAD profile data and commands. This includes:

General Behavior

For code examples, see the use cases below.

Initialzation

Useage

After plugging the callbacks shown above, and initializing the OAD module the application will begin receive callbacks related to OAD_QUEUE_EVT and OAD_DL_COMPLETE_EVT.

Processing OAD_QUEUE_EVT

Inside the application task function, the queue event should be processed:

// OAD events
if(events & OAD_QUEUE_EVT)
{
// Process the OAD Message Queue
uint8_t status = OAD_processQueue();
// If the OAD state machine encountered an error, print it
if(status == OAD_DL_COMPLETE)
{
//Display or print the message
}
else if(status == OAD_IMG_ID_TIMEOUT)
{
// Display the error and terminate the link
MAP_GAP_TerminateLinkReq(OAD_getactiveCxnHandle(),
}
else if(status != OAD_SUCCESS)
{
// Display the error
}
}

Processing OAD_DL_COMPLETE_EVT

At this time, the OAD is entirely complete and the system should be reset. The reset behavior is defined by the application.

Warning
The application should ensure the BLE-Stack has no pending items in its transmit buffer (i.e. final OAD response messages) before rebooting

Macro Definition Documentation

§ EXT_CTRL_OP_CODE

#define EXT_CTRL_OP_CODE (   pData)    (pData[0])

Macro to parse op-code from external control command

§ OAD_ATT_OVERHEAD

#define OAD_ATT_OVERHEAD   3

The ATT header overhead required to send a GATT_notifiation() This is used in calculating acceptable block sizes

§ OAD_BLK_NUM_HDR_SZ

#define OAD_BLK_NUM_HDR_SZ   4

The size of the OAD block number in a block write or block request

§ OAD_CCCD_CNT

#define OAD_CCCD_CNT   OAD_CHAR_CNT

Number of CCCDs in the OAD service

§ OAD_CHAR_CNT

#define OAD_CHAR_CNT   3

Number of characteristics in the OAD service

§ OAD_DEFAULT_BLOCK_SIZE

#define OAD_DEFAULT_BLOCK_SIZE   20

Minimum OAD block size OAD Block size can range from [OAD_DEFAULT_BLOCK_SIZE,OAD_MAX_BLOCK_SIZE]

Note
OAD block size must be 4 Octet aligned

§ OAD_DEFAULT_INACTIVITY_TIME

#define OAD_DEFAULT_INACTIVITY_TIME   10000

Default OAD inactivity timeout, the OAD state machine will cancel OAD if no activity is observed during this time.

The inactivity time is configurable via a parameter to OAD_open

§ OAD_EFL_MAX_META

#define OAD_EFL_MAX_META   4

Maximum number of external flash image header entries

Note
this only applies to off-chip OAD

§ OAD_EXT_CTRL_CMD_NOT_SUPPORTED

#define OAD_EXT_CTRL_CMD_NOT_SUPPORTED   0xFF

Error code returned when an external control command is received with an invalid opcode.

§ OAD_IMAGE_ID_RSP_LEN

#define OAD_IMAGE_ID_RSP_LEN   0x01

Size of the payload in an image identify response.

§ OAD_IMG_ID_RETRIES

#define OAD_IMG_ID_RETRIES   3

Number of failed image IDs are allowed before OAD terminates the cxn

§ OAD_IMG_INFO_ONCHIP

#define OAD_IMG_INFO_ONCHIP   0x01

There are two flavors of the get image info command:

  • A short get info command: returns the image info for the image on the chip
  • A long get info command: return an array of image info structures from external flash

§ OAD_IMG_PG_INVALID

#define OAD_IMG_PG_INVALID   0xFF

Invalid image page (outside of device flash)

§ OAD_MAX_BLOCK_SIZE

#define OAD_MAX_BLOCK_SIZE   244

Maximum OAD block size OAD Block size can range from [OAD_DEFAULT_BLOCK_SIZE,OAD_MAX_BLOCK_SIZE]

Note
OAD block size must be 4 Octet aligned

§ OAD_MIN_INACTIVITY_TIME

#define OAD_MIN_INACTIVITY_TIME   4000

Minimum OAD inactivity timeout, the OAD state machine will cancel OAD if no activity is observed during this time.

§ OAD_WRITE_PERMIT

#define OAD_WRITE_PERMIT   GATT_PERMIT_WRITE

This define controls whether the OAD profile requires BLE security By default, this is off.

Typedef Documentation

§ oadWriteCB_t

typedef void(* oadWriteCB_t) (uint8_t event, uint16_t arg)

OAD Module Write Callback Function

This callback is used to signal to the application that the OAD profile has received data over the air or needs to process an event in its internal queue

Parameters
eventThe event that the OAD module is posting in the application Can either OAD_QUEUE_EVT or OAD_DL_COMPLETE_EVT
argThis is the bim_var if performing on-chip OAD, otherwise unused

Enumeration Type Documentation

§ oadEvent_e

enum oadEvent_e

Event internal to the OAD module, use in state machine processing

Enumerator
OAD_WRITE_IDENTIFY_REQ 

Image identify received.

OAD_WRITE_BLOCK_REQ 

Image block request/response event.

OAD_IMAGE_COMPLETE 

OAD complete.

OAD_EXT_CTRL_WRITE_CMD 

External Control Command received.

OAD_TIMEOUT 

OAD peer timed out.

§ oadState_e

enum oadState_e

OAD state types

Enumerator
OAD_IDLE 

OAD module is not performing any action.

OAD_VALIDATE_IMG 

OAD module is checking an image.

OAD_CONFIG 

OAD module is configuring for a download.

OAD_DOWNLOAD 

OAD module is receiving an image.

OAD_CHECK_DL 

OAD module is validating an received image.

OAD_COMPLETE 

OAD module has completed a download.

Function Documentation

§ OAD_cancel()

void OAD_cancel ( void  )

Cancel and active OAD and reset the state

§ OAD_close()

void OAD_close ( void  )

Close the OAD and its flash_interface, reset the state

§ OAD_getactiveCxnHandle()

uint16_t OAD_getactiveCxnHandle ( )

Returns the active connection handle of the OAD session

Returns
handle - the 16-bit connection handle of the OAD session

§ OAD_getBlockSize()

uint16_t OAD_getBlockSize ( void  )

Gets the block size currently used by the OAD module

Returns
The block size being used.

§ OAD_getSWVersion()

bool OAD_getSWVersion ( uint8_t *  swVer,
uint8_t  len 
)

Returns the currently running SW version field

Parameters
swVer- pointer to array to copy version into
len- number of bytes to copy
Returns
status - true if copy succeeded
  • false if copy failed (invalid parameter)

§ OAD_isUsrAppValid()

bool OAD_isUsrAppValid ( void  )

Returns whether or not the user application is valid (on-chip OAD only)

Returns
user app status - true if the user app hasn't been erased.

§ OAD_open()

uint8_t OAD_open ( uint32_t  oadTimeout)

Open the OAD module

Initializes the OAD Service by registering GATT attributes with the GATT server. Only call this function once.

Parameters
oadTimeout- the timeout on for a pending OAD operation (in ms)
Returns
Success or Failure

§ OAD_processQueue()

uint8_t OAD_processQueue ( void  )

Process the OAD message queue/state machine

Returns
status of operation - OAD return status codes

§ OAD_register()

void OAD_register ( oadTargetCBs_t pfnOadCBs)

Register a callback function with the OAD Target Profile.

Parameters
pfnOadCBs- struct holding function pointers to OAD application callbacks oadTargetCBs_t

§ OAD_setBlockSize()

uint8_t OAD_setBlockSize ( uint16_t  mtuSize)

Sets the block size to be used during OAD based on a given MTU

Parameters
mtuSize- The negotiated MTU size
Returns
TRUE if operation is successful.

§ oadCreateFactoryImageBackup()

uint8_t oadCreateFactoryImageBackup ( void  )

This function creates factory image backup of current running image

Returns
OAD_SUCCESS on successful erasure else OAD_FLASH_ERR
Copyright 2018, Texas Instruments Incorporated