![]() |
![]() |
Timer driver interface.
The timer header file should be included in an application as follows:
The timer driver serves as the main interface for a typical RTOS application. Its purpose is to redirect the timer APIs to device specific implementations which are specified using a pointer to a Timer_FxnTable. The device specific implementations are responsible for creating all the RTOS specific primitives to allow for thead-safe operation. This driver does not have PWM or capture functionalities. These functionalities are addressed in both the capture and PWM driver.
The timer driver also handles the general purpose timer resource allocation. For each driver that requires use of a general purpose timer, it calls Timer_open() to occupy the specified timer, and calls Timer_close() to release the occupied timer resource.
The following example code opens a timer in continuous callback mode. The period is set to 1000 Hz.
In order to use the timer APIs, the application is required to provide device specific timer configuration in the Board.c file. The timer driver interface defines a configuration data structure:
The application must declare an array of Timer_Config elements, named Timer_config[]. Each element of Timer_config[] are populated with pointers to a device specific timer driver implementation's function table, driver object, and hardware attributes. The hardware attributes define properties such as the timer peripheral's base address, interrupt number and interrupt priority. Each element in Timer_config[] corresponds to a timer instance, and none of the elements should have NULL pointers. There is no correlation between the index and the peripheral designation (such as TIMER0 or TIMER1). For example, it is possible to use Timer_config[0] for TIMER1.
You will need to check the device specific timer driver implementation's header file for example configuration.
Timer_init() must be called before any other timer APIs. This function calls the device implementation's timer initialization function, for each element of Timer_config[].
The timer driver supports four modes of operation which may be specified in the Timer_Params.
Timer_ONESHOT_CALLBACK is non-blocking. After Timer_start() is called, the calling thread will continue execution. When the timer interrupt is triggered, the specified callback function will be called. The timer will not generate another interrupt unless Timer_start() is called again. Calling Timer_stop() or Timer_close() after Timer_start() but, before the timer interrupt, will prevent the specified callback from ever being invoked.
Timer_ONESHOT_BLOCKING is a blocking call. A semaphore is used to block the calling thead's execution until the timer generates an interrupt. If Timer_stop() is called, the calling thread will become unblocked immediately. The behavior of the timer in this mode is similar to a sleep function.
Timer_CONTINUOUS_CALLBACK is non-blocking. After Timer_start() is called, the calling thread will continue execution. When the timer interrupt is treiggered, the specified callback function will be called. The timer is automatically restarted and will continue to periodically generate interrupts until Timer_stop() is called.
Timer_FREE_RUNNING is non-blocking. After Timer_start() is called, the calling thread will continue execution. The timer will not generate an interrupt in this mode. The timer hardware will run until Timer_stop() is called.
The timer driver interface module is joined (at link time) to an array of Timer_Config data structures named Timer_config. Timer_config is implemented in the application with each entry being an instance of a timer peripheral. Each entry in Timer_config contains a:
The timer APIs are redirected to the device specific implementations using the Timer_FxnTable pointer of the Timer_config entry. In order to use device specific functions of the timer driver directly, link in the correct driver library for your device and include the device specific timer driver header file (which in turn includes Timer.h). For example, for the MSP432 family of devices, you would include the following header file:
#include <stdint.h>Go to the source code of this file.
Data Structures | |
| struct | Timer_Params_ |
| Timer Parameters. More... | |
| struct | Timer_FxnTable_ |
| The definition of a timer function table that contains the required set of functions to control a specific timer driver implementation. More... | |
| struct | Timer_Config_ |
| Timer Global configuration. More... | |
Macros | |
| #define | Timer_CMD_RESERVED (32) |
| #define | Timer_STATUS_RESERVED (-32) |
| #define | Timer_STATUS_SUCCESS (0) |
| Successful status code. More... | |
| #define | Timer_STATUS_ERROR (-1) |
| Generic error status code. More... | |
| #define | Timer_STATUS_UNDEFINEDCMD (-2) |
| An error status code returned by Timer_control() for undefined command codes. More... | |
| #define | TIMER_CMD_RESERVED Timer_CMD_RESERVED |
| #define | TIMER_STATUS_RESERVED Timer_STATUS_RESERVED |
| #define | TIMER_STATUS_SUCCESS Timer_STATUS_SUCCESS |
| #define | TIMER_STATUS_ERROR Timer_STATUS_ERROR |
| #define | TIMER_STATUS_UNDEFINEDCMD Timer_STATUS_UNDEFINEDCMD |
| #define | TIMER_ONESHOT_CB Timer_ONESHOT_CALLBACK |
| #define | TIMER_ONESHOT_BLOCK Timer_ONESHOT_BLOCKING |
| #define | TIMER_CONTINUOUS_CB Timer_CONTINUOUS_CALLBACK |
| #define | TIMER_MODE_FREE_RUNNING Timer_FREE_RUNNING |
| #define | TIMER_PERIOD_US Timer_PERIOD_US |
| #define | TIMER_PERIOD_HZ Timer_PERIOD_HZ |
| #define | TIMER_PERIOD_COUNTS Timer_PERIOD_COUNTS |
| #define | Timer_Period_Units Timer_PeriodUnits |
Typedefs | |
| typedef struct Timer_Config_ * | Timer_Handle |
| A handle that is returned from a Timer_open() call. More... | |
| typedef enum Timer_Mode_ | Timer_Mode |
| Timer mode settings. More... | |
| typedef enum Timer_PeriodUnits_ | Timer_PeriodUnits |
| Timer period unit enum. More... | |
| typedef void(* | Timer_CallBackFxn) (Timer_Handle handle) |
| Timer callback function. More... | |
| typedef struct Timer_Params_ | Timer_Params |
| Timer Parameters. More... | |
| typedef int_fast16_t(* | Timer_ControlFxn) (Timer_Handle handle, uint_fast16_t cmd, void *arg) |
| A function pointer to a driver specific implementation of Timer_control(). More... | |
| typedef void(* | Timer_CloseFxn) (Timer_Handle handle) |
| A function pointer to a driver specific implementation of Timer_close(). More... | |
| typedef uint32_t(* | Timer_GetCountFxn) (Timer_Handle handle) |
| A function pointer to a driver specific implementation of Timer_getCount(). More... | |
| typedef void(* | Timer_InitFxn) (Timer_Handle handle) |
| A function pointer to a driver specific implementation of Timer_init(). More... | |
| typedef Timer_Handle(* | Timer_OpenFxn) (Timer_Handle handle, Timer_Params *params) |
| A function pointer to a driver specific implementation of Timer_open(). More... | |
| typedef int32_t(* | Timer_StartFxn) (Timer_Handle handle) |
| A function pointer to a driver specific implementation of Timer_start(). More... | |
| typedef void(* | Timer_StopFxn) (Timer_Handle handle) |
| A function pointer to a driver specific implementation of Timer_stop(). More... | |
| typedef struct Timer_FxnTable_ | Timer_FxnTable |
| The definition of a timer function table that contains the required set of functions to control a specific timer driver implementation. More... | |
| typedef struct Timer_Config_ | Timer_Config |
| Timer Global configuration. More... | |
Enumerations | |
| enum | Timer_Mode_ { Timer_ONESHOT_CALLBACK, Timer_ONESHOT_BLOCKING, Timer_CONTINUOUS_CALLBACK, Timer_FREE_RUNNING } |
| Timer mode settings. More... | |
| enum | Timer_PeriodUnits_ { Timer_PERIOD_US, Timer_PERIOD_HZ, Timer_PERIOD_COUNTS } |
| Timer period unit enum. More... | |
Functions | |
| int_fast16_t | Timer_control (Timer_Handle handle, uint_fast16_t cmd, void *arg) |
| Function performs device specific features on a given Timer_Handle. More... | |
| void | Timer_close (Timer_Handle handle) |
| Function to close a timer. The corresponding timer to the Timer_Handle becomes an available timer resource. More... | |
| uint32_t | Timer_getCount (Timer_Handle handle) |
| Function to get the current count of a timer. More... | |
| void | Timer_init (void) |
| Function to initialize a timer module. This function will go through all available hardware resources and mark them as "available". More... | |
| Timer_Handle | Timer_open (uint_least8_t index, Timer_Params *params) |
| Function to initialize a given timer peripheral specified by the index argument. The Timer_Params specifies which mode the timer will operate. The accuracy of the desired period is limited by the the clock. For example, a 100 MHz clock will have a tick resolution of 10 nanoseconds. This function takes care of timer resource allocation. If the particular timer is available to use, the timer driver owns it and returns a Timer_Handle. More... | |
| void | Timer_Params_init (Timer_Params *params) |
| Function to initialize the Timer_Params struct to its defaults. More... | |
| int32_t | Timer_start (Timer_Handle handle) |
| Function to start the timer. More... | |
| void | Timer_stop (Timer_Handle handle) |
| Function to stop timer. If the timer is already stopped, this function has no effect. More... | |
| #define Timer_CMD_RESERVED (32) |
Common Timer_control command code reservation offset. Timer driver implementations should offset command codes with Timer_CMD_RESERVED growing positively
Example implementation specific command codes:
| #define Timer_STATUS_RESERVED (-32) |
Common Timer_control status code reservation offset. Timer driver implementations should offset status codes with Timer_STATUS_RESERVED growing negatively.
Example implementation specific status codes:
| #define Timer_STATUS_SUCCESS (0) |
Successful status code.
| #define Timer_STATUS_ERROR (-1) |
Generic error status code.
| #define Timer_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by Timer_control() for undefined command codes.
Timer_control() returns Timer_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.
| #define TIMER_CMD_RESERVED Timer_CMD_RESERVED |
| #define TIMER_STATUS_RESERVED Timer_STATUS_RESERVED |
| #define TIMER_STATUS_SUCCESS Timer_STATUS_SUCCESS |
| #define TIMER_STATUS_ERROR Timer_STATUS_ERROR |
| #define TIMER_STATUS_UNDEFINEDCMD Timer_STATUS_UNDEFINEDCMD |
| #define TIMER_ONESHOT_CB Timer_ONESHOT_CALLBACK |
| #define TIMER_ONESHOT_BLOCK Timer_ONESHOT_BLOCKING |
| #define TIMER_CONTINUOUS_CB Timer_CONTINUOUS_CALLBACK |
| #define TIMER_MODE_FREE_RUNNING Timer_FREE_RUNNING |
| #define TIMER_PERIOD_US Timer_PERIOD_US |
| #define TIMER_PERIOD_HZ Timer_PERIOD_HZ |
| #define TIMER_PERIOD_COUNTS Timer_PERIOD_COUNTS |
| #define Timer_Period_Units Timer_PeriodUnits |
| typedef struct Timer_Config_* Timer_Handle |
A handle that is returned from a Timer_open() call.
| typedef enum Timer_Mode_ Timer_Mode |
Timer mode settings.
This enum defines the timer modes that may be specified in Timer_Params.
| typedef enum Timer_PeriodUnits_ Timer_PeriodUnits |
Timer period unit enum.
This enum defines the units that may be specified for the period in Timer_Params.
| typedef void(* Timer_CallBackFxn) (Timer_Handle handle) |
Timer callback function.
User definable callback function prototype. The timer driver will call the defined function and pass in the timer driver's handle and the pointer to the user-specified the argument.
| handle | Timer_Handle |
| typedef struct Timer_Params_ Timer_Params |
Timer Parameters.
Timer parameters are used to with the Timer_open() call. Default values for these parameters are set using Timer_Params_init().
| typedef int_fast16_t(* Timer_ControlFxn) (Timer_Handle handle, uint_fast16_t cmd, void *arg) |
A function pointer to a driver specific implementation of Timer_control().
| typedef void(* Timer_CloseFxn) (Timer_Handle handle) |
A function pointer to a driver specific implementation of Timer_close().
| typedef uint32_t(* Timer_GetCountFxn) (Timer_Handle handle) |
A function pointer to a driver specific implementation of Timer_getCount().
| typedef void(* Timer_InitFxn) (Timer_Handle handle) |
A function pointer to a driver specific implementation of Timer_init().
| typedef Timer_Handle(* Timer_OpenFxn) (Timer_Handle handle, Timer_Params *params) |
A function pointer to a driver specific implementation of Timer_open().
| typedef int32_t(* Timer_StartFxn) (Timer_Handle handle) |
A function pointer to a driver specific implementation of Timer_start().
| typedef void(* Timer_StopFxn) (Timer_Handle handle) |
A function pointer to a driver specific implementation of Timer_stop().
| typedef struct Timer_FxnTable_ Timer_FxnTable |
The definition of a timer function table that contains the required set of functions to control a specific timer driver implementation.
| typedef struct Timer_Config_ Timer_Config |
Timer Global configuration.
The Timer_Config structure contains a set of pointers used to characterize the timer driver implementation.
This structure needs to be defined before calling Timer_init() and it must not be changed thereafter.
| enum Timer_Mode_ |
Timer mode settings.
This enum defines the timer modes that may be specified in Timer_Params.
| enum Timer_PeriodUnits_ |
Timer period unit enum.
This enum defines the units that may be specified for the period in Timer_Params.
| int_fast16_t Timer_control | ( | Timer_Handle | handle, |
| uint_fast16_t | cmd, | ||
| void * | arg | ||
| ) |
Function performs device specific features on a given Timer_Handle.
| handle | A Timer_Handle returned from Timer_open(). |
| cmd | A command value defined by the driver specific implementation. |
| arg | A pointer to an optional R/W (read/write) argument that is accompanied with cmd. |
| void Timer_close | ( | Timer_Handle | handle | ) |
Function to close a timer. The corresponding timer to the Timer_Handle becomes an available timer resource.
| handle | A Timer_Handle returned from Timer_open(). |
| uint32_t Timer_getCount | ( | Timer_Handle | handle | ) |
Function to get the current count of a timer.
| handle | A Timer_Handle returned from Timer_open(). |
| void Timer_init | ( | void | ) |
Function to initialize a timer module. This function will go through all available hardware resources and mark them as "available".
| Timer_Handle Timer_open | ( | uint_least8_t | index, |
| Timer_Params * | params | ||
| ) |
Function to initialize a given timer peripheral specified by the index argument. The Timer_Params specifies which mode the timer will operate. The accuracy of the desired period is limited by the the clock. For example, a 100 MHz clock will have a tick resolution of 10 nanoseconds. This function takes care of timer resource allocation. If the particular timer is available to use, the timer driver owns it and returns a Timer_Handle.
| index | Logical peripheral number for the Timer indexed into the Timer_config table. |
| params | Pointer to an parameter block, if NULL it will use default values. |
| void Timer_Params_init | ( | Timer_Params * | params | ) |
Function to initialize the Timer_Params struct to its defaults.
| params | A pointer to Timer_Params structure for initialization. |
Defaults values are: timerMode = Timer_ONESHOT_BLOCKING periodUnit = Timer_PERIOD_COUNTS timerCallback = NULL period = ~0
| int32_t Timer_start | ( | Timer_Handle | handle | ) |
Function to start the timer.
| handle | A Timer_Handle returned from Timer_open(). |
| void Timer_stop | ( | Timer_Handle | handle | ) |
Function to stop timer. If the timer is already stopped, this function has no effect.
| handle | A Timer_Handle returned from Timer_open(). |