![]() |
![]() |
BLE-Stack APIs
1.00.00
|
Parameter Structure for MITM Authentication data to be displayed. More...
Data Fields | |
uint8_t | display |
1 Byte TRUE if device must display passcode. | |
uint8_t | input |
1 Byte TRUE if device must input passcode. | |
uint32_t | numCmp |
32 bit Numeric Comparison value to display, 0 if not used. | |
Parameter Structure for MITM Authentication data to be displayed.
See SNP Event Indication for more information.
This is a packed structure. see Dealing with Parameters and Packed Structures for more information.