IEEE 802.15.4 Enable/Disable Source Matching Entry Command. More...
#include <rf_ieee_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x2003. More... | |
struct { | |
uint8_t bEnable:1 | |
0: Disable entry 1: Enable entry More... | |
uint8_t srcPend:1 | |
New value of the pending bit for the entry. More... | |
uint8_t entryType:1 | |
0: Extended address 1: Short address More... | |
} | options |
uint8_t | entryNo |
Index of entry to enable or disable. More... | |
IEEE 802.15.4 Enable/Disable Source Matching Entry Command.
uint8_t rfc_CMD_IEEE_MOD_SRC_MATCH_s::bEnable |
0: Disable entry
1: Enable entry
uint16_t rfc_CMD_IEEE_MOD_SRC_MATCH_s::commandNo |
The command ID number 0x2003.
uint8_t rfc_CMD_IEEE_MOD_SRC_MATCH_s::entryNo |
Index of entry to enable or disable.
uint8_t rfc_CMD_IEEE_MOD_SRC_MATCH_s::entryType |
0: Extended address
1: Short address
struct { ... } rfc_CMD_IEEE_MOD_SRC_MATCH_s::options |
uint8_t rfc_CMD_IEEE_MOD_SRC_MATCH_s::srcPend |
New value of the pending bit for the entry.