![]() |
![]() |
BLE-Stack APIs
3.00.01
|
Parameter Structure for SNP_UPDATE_CONN_PARAM_CNF. More...
Data Fields | |
uint16_t | connHandle |
handle of the connection the parameter update was intended for | |
uint8_t | status |
status of the request (SUCCESS or Error, list of status generated by the SNP.) | |
Parameter Structure for SNP_UPDATE_CONN_PARAM_CNF.
This does not mean parameters have been changed, only that the NP has successfully sent the request.
This is a packed structure. see Dealing with Parameters and Packed Structures for more information.