Abbreviation/Signal |
Type |
Description |
Signal |
Same as ACLK_REF |
|
Short |
Reference clock from OSC_TOP to AUX. Source is selectable. This clock signal can be used as an event in AUX |
|
Signal |
Internal Signal |
|
Short |
Audio Data line 0 |
|
Short |
Audio Data line 1 |
|
Short |
Audio Data line 2 |
|
Short |
Analog to Digital Converter |
|
Signal |
Internal Signal |
|
Short |
DMA trigger from the ADC, triggering DMA channel #7 |
|
Short |
ADC conversion done event available in AUX |
|
Short |
Event in AUX signaling that there is only room for one more sample in the ADC FIFO |
|
Short |
Event from ADC/ADC_FIFO to MCU domain. For details see user guide |
|
Short |
ADC reference voltage |
|
Module |
Analog to Digital Interface |
|
Short |
AMBA High-speed Bus |
|
Short |
Audio Inter Face |
|
Short |
Module controlling pins assigned to AUX |
|
Short |
Module controlling pins assigned to AUX |
|
Short |
Amplitude Compensation |
|
Short |
Voltage domain that is Always On |
|
Module |
Always on Event routing |
|
Module |
Always ON IOC |
|
Short |
Wake up event from AON to AUX. Up to three programmable sources OR'ed together to generate this event |
|
Module |
Always ON Real Time Clock |
|
Short |
Event from the AON_RTC channel 2 |
|
Short |
SW triggered event from AON to AUX |
|
Module |
Always ON WakeUp Control |
|
Short |
Advanced RISC Machines |
|
Signal |
Trace data bus for in ATB interface port 1. Connects to ETM when ETM is present. Connects to ITM when ETM does not exist. |
|
Signal |
Trace data bus for in ATB interface port 2. Connects to ITM when ETM is present. Tied-off when ETM does not exist. |
|
Short |
Analog Test |
|
Module |
AUX is the name of the Sensor Controller subsystem, it consists of a collection of modules used for simple tasks such as sensor communication. The modules can be used by both CPU and AUX_SCE. |
|
Short |
Module controlling pins assigned to AUX |
|
Short |
Module controlling pins assigned to AUX |
|
Short |
Combined event from AUX to MCU domain. See user guide for details |
|
Short |
Comparator A. Analog peripheral of AUX. In AUX this can also refer to the event coming from this comparator |
|
Short |
Comparator B. Analog peripheral of AUX. In AUX this can also refer to the event coming from this comparator |
|
Short |
AUX Sensor Controller Engine |
|
Short |
Analog/Digital General Purpose Input Output pin that can be mapped to AUX. For details see IOC |
|
Short |
Analog/Digital General Purpose Input Output pin that can be mapped to AUX. For details see IOC |
|
Short |
Analog/Digital General Purpose Input Output pin that can be mapped to AUX. For details see IOC |
|
Short |
Analog/Digital General Purpose Input Output pin that can be mapped to AUX. For details see IOC |
|
Short |
Analog/Digital General Purpose Input Output pin that can be mapped to AUX. For details see IOC |
|
Short |
Analog/Digital General Purpose Input Output pin that can be mapped to AUX. For details see IOC |
|
Short |
Analog/Digital General Purpose Input Output pin that can be mapped to AUX. For details see IOC |
|
Short |
Analog/Digital General Purpose Input Output pin that can be mapped to AUX. For details see IOC |
|
Short |
Analog/Digital General Purpose Input Output pin that can be mapped to AUX. For details see IOC |
|
Short |
Analog/Digital General Purpose Input Output pin that can be mapped to AUX. For details see IOC |
|
Short |
Analog/Digital General Purpose Input Output pin that can be mapped to AUX. For details see IOC |
|
Short |
Analog/Digital General Purpose Input Output pin that can be mapped to AUX. For details see IOC |
|
Short |
Analog/Digital General Purpose Input Output pin that can be mapped to AUX. For details see IOC |
|
Short |
Analog/Digital General Purpose Input Output pin that can be mapped to AUX. For details see IOC |
|
Short |
Analog/Digital General Purpose Input Output pin that can be mapped to AUX. For details see IOC |
|
Short |
Analog/Digital General Purpose Input Output pin that can be mapped to AUX. For details see IOC |
|
Short |
Special register in CPU used to prevent activation of exceptions based on their priority level |
|
Short |
Bit clock for the WCLK and serial audio data signals. This signal is an input when using an external clock source and output when using the internal clock source. |
|
Short |
Bus Fault Status Register |
|
Short |
CPU instruction, BreaKPoinT |
|
Short |
Interconnect or power domain including interconnect |
|
Short |
CPU instruction, Branch and eXchange instruction set |
|
Short |
Capture Compare PWM |
|
Module |
Power domain that contains clock management for MCU system |
|
Short |
||
Module |
Comparator A. |
|
Module |
Comparator B |
|
Short |
Special register in CPU used to control selector for main stack/process stack and selector for privileged/unpriviledged modes |
|
Short |
Cycles Per Instruction |
|
Short |
Central processing unit or power domain including system CPU |
|
Short |
Cyclical Redundancy Check algorithm |
|
Module |
Encryption engine |
|
Short |
Clear To Send, primary input to UART module from Ios |
|
Short |
Debug Access Port |
|
Module |
DCDC regulator for regulating VDDR |
|
Module |
Didital to Digital Interface |
|
Short |
DeepSleep Mode for CPU |
|
Short |
Digital IO |
|
Short |
Direct Memory Access |
|
Module |
Frequency doubling sub-module |
|
Short |
Single Phase Audio Interface Format |
|
Short |
||
Short |
Execution PSR |
|
Short |
Enhanced Trace Macrocell |
|
Module |
Event Fabric |
|
Signal |
A pre-defined value saved to LR on exception entry. This value indicates the required return stack and processor mode when returning from the exception |
|
Short |
Special register in CPU used to prevent activation of all exceptions except NMI |
|
Short |
First In First Out |
|
Module |
FLASH |
|
Module |
Flash Memory Controller |
|
Short |
||
Module |
Free Running Oscillator |
|
Short |
Finite State Machine |
|
Short |
Serial Frame signal for SSI interface |
|
Module |
||
Module |
General Purpose Input/Output |
|
Short |
General Purpose RAM |
|
Module |
General Purpose Timer |
|
Module |
GPT module 0 |
|
Module |
GPT module 1 |
|
Module |
GPT module 2 |
|
Module |
GPT module 3 |
|
Short |
High Frequency |
|
Signal |
State |
|
Short |
Hardware |
|
Module |
Inter-Integrated Circuit, a multimaster serial single-ended computer bus |
|
Module |
Inter-IC Sound, audio interface |
|
Short |
IDentification number |
|
Signal |
State |
|
Module |
Intermediate Frequency Analog to Digital Converter |
|
Module |
Intermediate Frequency AMPlifier |
|
Short |
Input/Output |
|
Module |
Input/Output Configurator |
|
Short |
Interrupt PSR |
|
Short |
Current Proportional to Absolute Temperature |
|
Short |
Interrupt Service Routine |
|
Short |
Current source |
|
Signal |
This signal clamps the output of the current source. The signal can also be used as an event in AUX |
|
Short |
CPU instruction, IF-THEN |
|
Short |
Instrumentation Trace Macrocell |
|
Short |
Joint Test Action Group. The name of the organization that developed standard IEEE 1149.1. This standard defines a boundary-scan architecture used for in-circuit testing of integrated circuit devices. It is commonly known by the initials JTAG. |
|
Short |
CPU instruction, Load Multiple |
|
Short |
Low Drop-Out voltage regulator |
|
Short |
CPU instruction, Load Register |
|
Short |
CPU instruction, Doubleword Load Register |
|
Short |
Linear Feedback Shift Register |
|
Short |
Dual Phased Left Justified Audio Interface Format |
|
Short |
Low-Noise Amplifier |
|
Signal |
State |
|
Short |
Link Register 12 from Cortex M Processor |
|
Short |
Least Significant Bit |
|
Short |
Load Store Unit |
|
Short |
Least Significant Word |
|
Short |
High-speed master clock used for sample conversion in the external audio device. This signal is not unused when using an external clock source. |
|
Short |
Microcontroller Unit |
|
Short |
Power doamin that is always powered when MCU voltage domain is powered |
|
Module |
Always on interface module |
|
Short |
Event from MCU domain to AUX. Source is configurable in event fabric |
|
Short |
Undivided MCU system clock |
|
Short |
Memory Manage Fault Status Register |
|
Short |
Memory Protection Unit |
|
Short |
CPU instruction, Move the contents of a special register to a general-purpose register |
|
Short |
Most Significant Bit |
|
Short |
Main Stack Pointer |
|
Short |
Most Significant Word |
|
Short |
Non-Maskable Interrupt |
|
Short |
Non Return-to-Zero |
|
Short |
Nested Vectored Interrupt Controller |
|
Short |
In AUX this refers to bit 0 of the signals that can be routed from the observability mux to AUX |
|
Short |
In AUX this refers to bit 1 of the signals that can be routed from the observability mux to AUX |
|
Short |
In AUX this refers to bit 2 of the signals that can be routed from the observability mux to AUX |
|
Short |
In AUX this refers to bit 3 of the signals that can be routed from the observability mux to AUX |
|
Short |
Oscillator (see also ANAOSC) |
|
Module |
Oscillators Digital control |
|
Module |
Power Amplifier |
|
Short |
Program Counter |
|
Short |
Power domain including peripheral modules |
|
Short |
CPU instruction, Pop register(s) off the stack |
|
Short |
Parts Per Million |
|
Module |
Power Reset Clock Manager |
|
Short |
Special register in CPU used to prevent activation of all exceptions with configurable priority |
|
Short |
Process Stack Pointer |
|
Short |
Program Status Register |
|
Short |
Pulse Width Modulation |
|
Short |
General-purpose Register 0 from Cortex M Processor |
|
Short |
General-purpose Register 1 from Cortex M Processor |
|
Short |
General-purpose Register 10 from Cortex M Processor |
|
Short |
General-purpose Register 11 from Cortex M Processor |
|
Short |
General-purpose Register 12 from Cortex M Processor |
|
Short |
General-purpose Register 2 from Cortex M Processor |
|
Short |
General-purpose Register 3 from Cortex M Processor |
|
Short |
General-purpose Register 4 from Cortex M Processor |
|
Short |
General-purpose Register 5 from Cortex M Processor |
|
Short |
General-purpose Register 6 from Cortex M Processor |
|
Short |
General-purpose Register 7 from Cortex M Processor |
|
Short |
General-purpose Register 8 from Cortex M Processor |
|
Short |
General-purpose Register 9 from Cortex M Processor |
|
Short |
||
Short |
RC Oscillator |
|
Signal |
RC-oscillator High Frequency module or the clock signal outputted by this module |
|
Short |
RC Oscillator, High Frequency |
|
Short |
RC Oscillator, Low Frequency |
|
Short |
See rcosc_hf |
|
Short |
Reference System. Module generating refernce voltages and reference currents for use in analog blocks. |
|
Module |
Radio Frequency |
|
Module |
RF Core |
|
Module |
RF Engine |
|
Short |
Dual Phased Right Justified Audio Interface Format |
|
Short |
Read Only Memory |
|
Short |
Real Time Clock |
|
Short |
4 kHz signal coming from the RTC counter. Can be used by timers in AUX |
|
Short |
Event that goes high every time the RTC channel 2 generates an event |
|
Signal |
16 KHz signal used to synchronize the radio timer to RTC |
|
Short |
Real-Time Operating System |
|
Short |
Request To Send, primary output from UART module to Ios |
|
Short |
Receive |
|
Short |
||
Short |
Successive Approximation Register (used for Binary Search) |
|
short |
Serial CLock, I2C clock line |
|
Signal |
System Clock High Frequency |
|
Short |
System Clock, High Frequency |
|
Signal |
System Clock, Low Frequency |
|
Short |
System Clock, Low Frequency |
|
Signal |
||
Short |
CPU instruction, Signed Divide |
|
Short |
Power domain including serial modules |
|
Short |
CPU instruction, Send Event |
|
Short |
Lowest possible powermode, where all but the VDDS domain is powered off |
|
Short |
Serial Modem Interface |
|
Short |
A semaphore has been released to AUX_SCE using the AUTOTAKE feature in AUX_SMPH module |
|
Short |
Stack Pointer |
|
Short |
Serial Peripheral Interface |
|
Short |
Static Random Access Memory |
|
Short |
Synchronous Serial Interface |
|
Module |
Instance 0 of SSI Module |
|
Module |
Instance 1 of SSI Module |
|
Short |
CPU instruction, Store Multiple |
|
Short |
CPU instruction, Doubleword Store Register |
|
Short |
CPU instruction, Supervisor Call |
|
Short |
Software |
|
Short |
SW triggered event 0 from AUX to AON. Triggered by writes to AUX_EVCTL:SWEVSET |
|
Short |
SW triggered event 1 from AUX to AON. Triggered by writes to AUX_EVCTL:SWEVSET |
|
Short |
SW triggered event 2 from AUX to AON. Triggered by writes to AUX_EVCTL:SWEVSET |
|
Short |
Serial Wire Output |
|
Signal |
Serial Wire Viewer Debug Signal from CPU Module |
|
Short |
CPU system bus |
|
Short |
Test Access Port |
|
Signal |
JTAG compliant pin (test clock) |
|
Short |
Time to Digital Converter |
|
Short |
Time to Digital Conversion done. Event available in AUX |
|
Signal |
Time to digital prescaler output. Can be used as an event in the TDC |
|
Short |
Texas Instruments |
|
Short |
Event from timer0 in AUX. Event triggered when timer count >= target value |
|
Short |
Event from timer1 in AUX. Event triggered when timer count >= target value |
|
Short |
Trace Port Analyzer |
|
Short |
||
Module |
True Random Number Generator |
|
Short |
Transmit |
|
Short |
||
Short |
Universal Asynchronous Receiver/Transmitter |
|
Module |
Instance 0 of UART Module |
|
Short |
Receive input, Primary input to UART module from Ios |
|
Short |
Transmit output, Primary output from UART module to Ios |
|
Short |
CPU instruction, Unsigned Divide |
|
Module |
Micro DMA |
|
Short |
||
Short |
Usage Fault Status Register |
|
Module |
Micropower Low Drop-out Voltage Regulator |
|
Signal |
Regulated supply voltage for digital domain. |
|
Signal |
Regulated (1.7V?) supply voltage. |
|
Signal |
Main supply voltage (battery). |
|
Short |
Power domain including Flash memory |
|
Short |
Sample framing signal/clock that defines the sample frequency and the word boundaries in the serial data stream. The WCLK frequency is identical to the sample frequency. This signal is an input when using an external clock source and output when using the internal clock source. |
|
Module |
Watch Dog Timer |
|
Short |
CPU instruction, Wait For Event |
|
Short |
CPU instruction, Wait For Interrupt |
|
Module |
Wakeup Interrupt Controller |
|
Module |
Wake Up Controller |
|
Short |
eXecute Never |
|
Short |
Crystal Oscillator |
|
Signal |
See XOSC_HF |
|
Short |
Crystal Oscillator, High Frequency |
|
Signal |
See XOSC_LF |
|
Short |
Crystal Oscillator, Low Frequency |
|
Short |
See XOSC_HF |
|
Short |
Program Status Register |
|
Short |
Crystal |