#include <rf_ble_cmd.h>
Data Fields | |
dataQueue_t * | pRxQ |
Pointer to receive queue. More... | |
struct { | |
uint8_t bAutoFlushIgnored:1 | |
If 1, automatically remove ignored packets from Rx queue. More... | |
uint8_t bAutoFlushCrcErr:1 | |
If 1, automatically remove packets with CRC error from Rx queue. More... | |
uint8_t bAutoFlushEmpty:1 | |
If 1, automatically remove empty packets from Rx queue. More... | |
uint8_t bIncludeLenByte:1 | |
If 1, include the received length byte in the stored packet; otherwise discard it. More... | |
uint8_t bIncludeCrc:1 | |
If 1, include the received CRC field in the stored packet; otherwise discard it. More... | |
uint8_t bAppendRssi:1 | |
If 1, append an RSSI byte to the packet in the Rx queue. More... | |
uint8_t bAppendStatus:1 | |
If 1, append a status word to the packet in the Rx queue. More... | |
uint8_t bAppendTimestamp:1 | |
If 1, append a timestamp to the packet in the Rx queue. More... | |
} | rxConfig |
Configuration bits for the receive queue entries. More... | |
struct { | |
uint8_t advFilterPolicy:2 | |
Advertiser filter policy 0: Process scan and connect requests from all devices 1: Process connect requests from all devices and only scan requests from devices that are in the white list 2: Process scan requests from all devices and only connect requests from devices that are in the white list 3: Process scan and connect requests only from devices in the white list. More... | |
uint8_t deviceAddrType:1 | |
The type of the device address – public (0) or random (1) More... | |
uint8_t peerAddrType:1 | |
Directed advertiser: The type of the peer address – public (0) or random (1) More... | |
uint8_t bStrictLenFilter:1 | |
0: Accept any packet with a valid advertising packet length 1: Discard messages with illegal length for the given packet type More... | |
uint8_t __pad0__:2 | |
uint8_t rpaMode:1 | |
Resolvable private address mode 0: Normal operation 1: Use white list for a received RPA regardless of filter policy. More... | |
} | advConfig |
uint8_t | advLen |
Size of advertiser data. More... | |
uint8_t | scanRspLen |
Size of scan response data. More... | |
uint8_t * | pAdvData |
Pointer to buffer containing ADV*_IND data. More... | |
uint8_t * | pScanRspData |
Pointer to buffer containing SCAN_RSP data. More... | |
uint16_t * | pDeviceAddress |
Pointer (with least significant bit set to 0) to device address used for this device. If least significant bit is 1, the address type given by advConfig.deviceAddrType is inverted. More... | |
rfc_bleWhiteListEntry_t * | pWhiteList |
Pointer (with least significant bit set to 0) to white list or peer address (directed advertiser). If least significant bit is 1, the address type given by advConfig.peerAddrType is inverted. More... | |
uint16_t | __dummy0 |
uint8_t | __dummy1 |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | endTrigger |
Trigger that causes the device to end the advertiser event as soon as allowed. More... | |
ratmr_t | endTime |
Time used together with endTrigger that causes the device to end the advertiser event as soon as allowed. More... | |
uint16_t rfc_bleAdvPar_s::__dummy0 |
uint8_t rfc_bleAdvPar_s::__dummy1 |
uint8_t rfc_bleAdvPar_s::__pad0__ |
struct { ... } rfc_bleAdvPar_s::advConfig |
uint8_t rfc_bleAdvPar_s::advFilterPolicy |
Advertiser filter policy
0: Process scan and connect requests from all devices
1: Process connect requests from all devices and only scan requests from devices that are in the white list
2: Process scan requests from all devices and only connect requests from devices that are in the white list
3: Process scan and connect requests only from devices in the white list.
uint8_t rfc_bleAdvPar_s::advLen |
Size of advertiser data.
uint8_t rfc_bleAdvPar_s::bAppendRssi |
If 1, append an RSSI byte to the packet in the Rx queue.
uint8_t rfc_bleAdvPar_s::bAppendStatus |
If 1, append a status word to the packet in the Rx queue.
uint8_t rfc_bleAdvPar_s::bAppendTimestamp |
If 1, append a timestamp to the packet in the Rx queue.
uint8_t rfc_bleAdvPar_s::bAutoFlushCrcErr |
If 1, automatically remove packets with CRC error from Rx queue.
uint8_t rfc_bleAdvPar_s::bAutoFlushEmpty |
If 1, automatically remove empty packets from Rx queue.
uint8_t rfc_bleAdvPar_s::bAutoFlushIgnored |
If 1, automatically remove ignored packets from Rx queue.
uint8_t rfc_bleAdvPar_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
uint8_t rfc_bleAdvPar_s::bIncludeCrc |
If 1, include the received CRC field in the stored packet; otherwise discard it.
uint8_t rfc_bleAdvPar_s::bIncludeLenByte |
If 1, include the received length byte in the stored packet; otherwise discard it.
uint8_t rfc_bleAdvPar_s::bStrictLenFilter |
0: Accept any packet with a valid advertising packet length
1: Discard messages with illegal length for the given packet type
uint8_t rfc_bleAdvPar_s::deviceAddrType |
The type of the device address – public (0) or random (1)
ratmr_t rfc_bleAdvPar_s::endTime |
Time used together with endTrigger
that causes the device to end the advertiser event as soon as allowed.
struct { ... } rfc_bleAdvPar_s::endTrigger |
Trigger that causes the device to end the advertiser event as soon as allowed.
uint8_t* rfc_bleAdvPar_s::pAdvData |
Pointer to buffer containing ADV*_IND data.
uint8_t rfc_bleAdvPar_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
uint16_t* rfc_bleAdvPar_s::pDeviceAddress |
Pointer (with least significant bit set to 0) to device address used for this device. If least significant bit is 1, the address type given by advConfig.deviceAddrType
is inverted.
uint8_t rfc_bleAdvPar_s::peerAddrType |
Directed advertiser: The type of the peer address – public (0) or random (1)
dataQueue_t* rfc_bleAdvPar_s::pRxQ |
Pointer to receive queue.
uint8_t* rfc_bleAdvPar_s::pScanRspData |
Pointer to buffer containing SCAN_RSP data.
rfc_bleWhiteListEntry_t* rfc_bleAdvPar_s::pWhiteList |
Pointer (with least significant bit set to 0) to white list or peer address (directed advertiser). If least significant bit is 1, the address type given by advConfig.peerAddrType
is inverted.
uint8_t rfc_bleAdvPar_s::rpaMode |
Resolvable private address mode
0: Normal operation
1: Use white list for a received RPA regardless of filter policy.
struct { ... } rfc_bleAdvPar_s::rxConfig |
Configuration bits for the receive queue entries.
uint8_t rfc_bleAdvPar_s::scanRspLen |
Size of scan response data.
uint8_t rfc_bleAdvPar_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
uint8_t rfc_bleAdvPar_s::triggerType |
The type of trigger.