|
void | UARTFIFOLevelGet (uint32_t ui32Base, uint32_t *pui32TxLevel, uint32_t *pui32RxLevel) |
| Gets the FIFO level at which interrupts are generated. More...
|
|
void | UARTConfigSetExpClk (uint32_t ui32Base, uint32_t ui32UARTClk, uint32_t ui32Baud, uint32_t ui32Config) |
| Sets the configuration of a UART. More...
|
|
void | UARTConfigGetExpClk (uint32_t ui32Base, uint32_t ui32UARTClk, uint32_t *pui32Baud, uint32_t *pui32Config) |
| Gets the current configuration of a UART. More...
|
|
void | UARTDisable (uint32_t ui32Base) |
| Disables transmitting and receiving. More...
|
|
int32_t | UARTCharGetNonBlocking (uint32_t ui32Base) |
| Receives a character from the specified port. More...
|
|
int32_t | UARTCharGet (uint32_t ui32Base) |
| Waits for a character from the specified port. More...
|
|
bool | UARTCharPutNonBlocking (uint32_t ui32Base, uint8_t ui8Data) |
| Sends a character to the specified port. More...
|
|
void | UARTCharPut (uint32_t ui32Base, uint8_t ui8Data) |
| Waits to send a character from the specified port. More...
|
|
void | UARTIntRegister (uint32_t ui32Base, void(*pfnHandler)(void)) |
| Registers an interrupt handler for a UART interrupt. More...
|
|
void | UARTIntUnregister (uint32_t ui32Base) |
| Unregisters an interrupt handler for a UART interrupt. More...
|
|