CC26xx Driver Library
rfc_bleScannerPar_s Struct Reference

#include <rf_ble_cmd.h>

Data Fields

dataQueue_tpRxQ
 Pointer to receive queue. More...
 
struct {
   uint8_t   bAutoFlushIgnored:1
 If 1, automatically remove ignored packets from Rx queue. More...
 
   uint8_t   bAutoFlushCrcErr:1
 If 1, automatically remove packets with CRC error from Rx queue. More...
 
   uint8_t   bAutoFlushEmpty:1
 If 1, automatically remove empty packets from Rx queue. More...
 
   uint8_t   bIncludeLenByte:1
 If 1, include the received length byte in the stored packet; otherwise discard it. More...
 
   uint8_t   bIncludeCrc:1
 If 1, include the received CRC field in the stored packet; otherwise discard it. More...
 
   uint8_t   bAppendRssi:1
 If 1, append an RSSI byte to the packet in the Rx queue. More...
 
   uint8_t   bAppendStatus:1
 If 1, append a status byte to the packet in the Rx queue. More...
 
   uint8_t   bAppendTimestamp:1
 If 1, append a timestamp to the packet in the Rx queue. More...
 
rxConfig
 Configuration bits for the receive queue entries. More...
 
struct {
   uint8_t   scanFilterPolicy:1
 Scanning filter policy
0: Accept all advertisement packets
1: Accept only advertisement packets from devices where the advertiser's address is in the White list. More...
 
   uint8_t   bActiveScan:1
 0: Passive scan
1: Active scan More...
 
   uint8_t   deviceAddrType:1
 The type of the device address – public (0) or random (1) More...
 
   uint8_t   __pad0__:1
 
   uint8_t   bStrictLenFilter:1
 0: Accept any packet with a valid advertising packet length
1: Discard messages with illegal length for the given packet type More...
 
   uint8_t   bAutoWlIgnore:1
 1: Automatically set ignore bit in white list More...
 
   uint8_t   bEndOnRpt:1
 0: Continue scanner operation after each reporting ADV*_IND or sending SCAN_RSP
1: End scanner operation after each reported ADV*_IND and potentially SCAN_RSP More...
 
   uint8_t   rpaMode:1
 Resolvable private address mode
0: Normal operation
1: Use white list for a received RPA regardless of filter policy. More...
 
scanConfig
 
uint16_t randomState
 State for pseudo-random number generation used in backoff procedure. More...
 
uint16_t backoffCount
 Parameter backoffCount used in backoff procedure, cf. Bluetooth 4.0 spec. More...
 
struct {
   uint8_t   logUpperLimit:4
 Binary logarithm of parameter upperLimit used in scanner backoff procedure. More...
 
   uint8_t   bLastSucceeded:1
 1 if the last SCAN_RSP was successfully received and upperLimit not changed More...
 
   uint8_t   bLastFailed:1
 1 if reception of the last SCAN_RSP failed and upperLimit was not changed More...
 
backoffPar
 
uint8_t scanReqLen
 Size of scan request data. More...
 
uint8_t * pScanReqData
 Pointer to buffer containing SCAN_REQ data. More...
 
uint16_t * pDeviceAddress
 Pointer to device address used for this device. More...
 
rfc_bleWhiteListEntry_tpWhiteList
 Pointer to white list. More...
 
uint16_t __dummy0
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
timeoutTrigger
 Trigger that causes the device to stop receiving as soon as allowed. More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
endTrigger
 Trigger that causes the device to stop receiving as soon as allowed. More...
 
ratmr_t timeoutTime
 Time used together with timeoutTrigger that causes the device to stop receiving as soon as allowed, ending with BLE_DONE_RXTIMEOUT. More...
 
ratmr_t endTime
 Time used together with endTrigger that causes the device to stop receiving as soon as allowed, ending with BLE_DONE_ENDED. More...
 

Field Documentation

uint16_t rfc_bleScannerPar_s::__dummy0
uint8_t rfc_bleScannerPar_s::__pad0__
uint16_t rfc_bleScannerPar_s::backoffCount

Parameter backoffCount used in backoff procedure, cf. Bluetooth 4.0 spec.

struct { ... } rfc_bleScannerPar_s::backoffPar
uint8_t rfc_bleScannerPar_s::bActiveScan

0: Passive scan
1: Active scan

uint8_t rfc_bleScannerPar_s::bAppendRssi

If 1, append an RSSI byte to the packet in the Rx queue.

uint8_t rfc_bleScannerPar_s::bAppendStatus

If 1, append a status byte to the packet in the Rx queue.

uint8_t rfc_bleScannerPar_s::bAppendTimestamp

If 1, append a timestamp to the packet in the Rx queue.

uint8_t rfc_bleScannerPar_s::bAutoFlushCrcErr

If 1, automatically remove packets with CRC error from Rx queue.

uint8_t rfc_bleScannerPar_s::bAutoFlushEmpty

If 1, automatically remove empty packets from Rx queue.

uint8_t rfc_bleScannerPar_s::bAutoFlushIgnored

If 1, automatically remove ignored packets from Rx queue.

uint8_t rfc_bleScannerPar_s::bAutoWlIgnore

1: Automatically set ignore bit in white list

uint8_t rfc_bleScannerPar_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

uint8_t rfc_bleScannerPar_s::bEndOnRpt

0: Continue scanner operation after each reporting ADV*_IND or sending SCAN_RSP
1: End scanner operation after each reported ADV*_IND and potentially SCAN_RSP

uint8_t rfc_bleScannerPar_s::bIncludeCrc

If 1, include the received CRC field in the stored packet; otherwise discard it.

uint8_t rfc_bleScannerPar_s::bIncludeLenByte

If 1, include the received length byte in the stored packet; otherwise discard it.

uint8_t rfc_bleScannerPar_s::bLastFailed

1 if reception of the last SCAN_RSP failed and upperLimit was not changed

uint8_t rfc_bleScannerPar_s::bLastSucceeded

1 if the last SCAN_RSP was successfully received and upperLimit not changed

uint8_t rfc_bleScannerPar_s::bStrictLenFilter

0: Accept any packet with a valid advertising packet length
1: Discard messages with illegal length for the given packet type

uint8_t rfc_bleScannerPar_s::deviceAddrType

The type of the device address – public (0) or random (1)

ratmr_t rfc_bleScannerPar_s::endTime

Time used together with endTrigger that causes the device to stop receiving as soon as allowed, ending with BLE_DONE_ENDED.

struct { ... } rfc_bleScannerPar_s::endTrigger

Trigger that causes the device to stop receiving as soon as allowed.

uint8_t rfc_bleScannerPar_s::logUpperLimit

Binary logarithm of parameter upperLimit used in scanner backoff procedure.

uint8_t rfc_bleScannerPar_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

uint16_t* rfc_bleScannerPar_s::pDeviceAddress

Pointer to device address used for this device.

dataQueue_t* rfc_bleScannerPar_s::pRxQ

Pointer to receive queue.

uint8_t* rfc_bleScannerPar_s::pScanReqData

Pointer to buffer containing SCAN_REQ data.

rfc_bleWhiteListEntry_t* rfc_bleScannerPar_s::pWhiteList

Pointer to white list.

uint16_t rfc_bleScannerPar_s::randomState

State for pseudo-random number generation used in backoff procedure.

uint8_t rfc_bleScannerPar_s::rpaMode

Resolvable private address mode
0: Normal operation
1: Use white list for a received RPA regardless of filter policy.

struct { ... } rfc_bleScannerPar_s::rxConfig

Configuration bits for the receive queue entries.

struct { ... } rfc_bleScannerPar_s::scanConfig
uint8_t rfc_bleScannerPar_s::scanFilterPolicy

Scanning filter policy
0: Accept all advertisement packets
1: Accept only advertisement packets from devices where the advertiser's address is in the White list.

uint8_t rfc_bleScannerPar_s::scanReqLen

Size of scan request data.

ratmr_t rfc_bleScannerPar_s::timeoutTime

Time used together with timeoutTrigger that causes the device to stop receiving as soon as allowed, ending with BLE_DONE_RXTIMEOUT.

struct { ... } rfc_bleScannerPar_s::timeoutTrigger

Trigger that causes the device to stop receiving as soon as allowed.

uint8_t rfc_bleScannerPar_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

uint8_t rfc_bleScannerPar_s::triggerType

The type of trigger.