The CC13xx Driver Library from Texas Instruments® (also referred to as "DriverLib") is a set of drivers for accessing the peripherals found on the CC13xx family of ARM® Cortex™-M3 based devices. The DriverLib functions are grouped in APIs based on either specific on-chip peripheral module (e.g. SPI, UART, etc ) or more general functionality (e.g. system control, oscillator settings, etc). Each API uses a unique pre-fix for all the DriverLib functions in that API to indicate which module or type of functionality being accessed (with a few exceptions).
The capabilities and organization of the drivers are governed by the following design goals:
Some consequences of these design goals are:
For many applications the drivers can be used as is. But in some cases the drivers must be enhanced or rewritten to meet the functionality, memory, or processing requirements of the application. If so, the existing driver can be used as a reference on how to operate the peripheral.
A brief overview of the organization of the driver library source code follows:
driverlib/
inc/
Currently, DriverLib source code supports the following tools:
Besides the source code for the driver library Texas Instruments also provides pre-compiled libraries of the driver library. These libraries are found in driverlib/bin/.
Currently, pre-compiled libraries are provided for the following tools:
DriverLib provides support for two programming models:
Each model can be used independently or combined, based on the needs of the application or the programming environment desired by the developer.
Each programming model has advantages and disadvantages. Use of the direct register access model generally results in smaller and more efficient code than using the software driver model. However, the direct register access model requires detailed knowledge of the operation of each register and bit field, as well as their interactions and any sequencing required for proper operation of the peripheral; the software driver model insulates the developer from these details, thus generally requiring less time to develop applications.
In the direct register access model, the peripherals are programmed by the application by writing values directly into the registers in the peripheral. A set of defines, that simplify this process, is provided.
These defines are located in the inc/ directory and there is a single hw_<module>.h header file for each peripheral type. For example, the defines for SSI are located in the hw_ssi.h header file.
The defines used by the direct register access model follow a naming convention that makes it easier to know how to use a particular macro. The rules are as follows:
SSI for the SSI module) and are followed by the name of the register as it appears in the data sheet._O_ (for example, CR0 register in the data sheet results in SSI_O_CR0). The base address of each peripheral is defined in the memory map header file located in the inc/ directory, with the name hw_memmap.h.hw_ssi.h file for the SSI registers).SCR bit field in the CR0 register in the SSI module is identified by SSI_CR0_SCR...._M represent the mask for a bit field in a register._S represent the number of bits to shift a value in order to align it with a bit field. These values match the macro with the same base name but ending with _M._BITN have the same value as _S but are only defined for single-bit bit fields thus representing the bit number. These defines should be used for bit band operations to ensure that only single-bit bit fields are accessed._W represent the width of the bit field.SSI_CR0_DSS bit field has a set of enumerations that specify the allowed values of this bit field pre-shifted to the correct bit positions. E.g. the enumeration "7_BIT" can be set using the define SSI_CR0_DSS_7_BIT. This improves readability and also helps the programmer select valid values for specific bit fields.A set of macros is provided in hw_types.h to use together with the register defines to read and write the corresponding addresses:
Given these defines and macros, the CR0 register, in the first instance of the SSI peripheral (SSI0), can be programmed as follows:
HWREG(SSI0_BASE + SSI_O_CR0) = ((5 << SSI_CR0_SCR_S) | SSI_CR0_SPH | SSI_CR0_SPO);
Alternatively, the following has the same effect (although it is not as easy to understand):
HWREG(SSI0_BASE + SSI_O_CR0) = 0x000005c0;
The value of the SCR field from the CR0 register can be extracted as follows:
ulValue = (HWREG(SSI0_BASE + SSI_O_CR0) & SSI_CR0_SCR_M) >> SSI_CR0_SCR_S;
The device supports ARM's so-called "bit-band operations" which is a mechanism that makes a read-modify-write operation an atomic operation seen from the CPU's perspective. I.e. the CPU can write a single bit in a register/memory without executing the usual read-modify-write operation but instead the CPU only needs to perform a single write operation, and then the bus performs the actual read-modify-write towards the memory or peripheral module. Same goes for reading single bits as the bus takes care of masking and shifting such that the CPU receives a word only containing the bit of interest located at the LSB.
Bit-band operations are only possible in the bit-band regions where the LSB of each word represents a single bit in a bit-band alias region. The term "bit-band alias" describes the registers or memory locations to which the bus performs the actual read-modify-write operation. In other words, if a programmer wants to perform a bit operation on a register, the register must be in the bit-band alias region, and then he can perform a bit-band operation to the bit-band region and then the bus remaps it to the bit-band alias address.
The provided macros, HWREGBITW etc, "hide" the bit-band regions to the programmer such that the programmer only needs to program which bit of a register (in the bit-band alias region) he wants to write or read. Thus the macro maps the register and bit number to an address in the bit-band region and then the bus performs the bit-band operation by remapping back to the bit-band alias address.
The device has two bit-band alias regions, each spanning 1MB, which are:
0x2000_0000 - 0x200F_FFFF0x4000_0000 - 0x400F_FFFFThe corresponding bit-band regions, each spanning 32MB, (accessed through the macros) are:
0x2200_0000 - 0x23FF_FFFF0x4200_0000 - 0x43FF_FFFFThus, instead of using the usual read-modify-write to clear a bit:
HWREG(SSI0_BASE + SSI_O_CR0) &= ~(SSI_CR0_SPO_M);
it is possible to use bit-banding:
HWREGBITW(SSI0_BASE + SSI_O_CR0, SSI_CR0_SPO_BITN) = 0;
In the software driver model, the APIs provided in DriverLib are used by applications to control the peripherals. Because these drivers provide complete control of the peripherals in their normal mode of operation, it is possible to write an entire application without direct access to the hardware. This method provides for rapid development of the application without requiring knowledge of how to program the peripheral registers.
Corresponding to the direct register access model example, the following call also programs the CR0 register in the SSI module (though the register name is hidden by the API):
SSIConfigSetExpClk(SSI0_BASE, 50000000, SSI_FRF_MOTO_MODE_3,
SSI_MODE_MASTER, 1000000, 8);
The resulting value in the CR0 register might not be exactly the same because SSIConfigSetExpClk() may compute a different value for the SCR bit field than what was used in the direct register access model example.
The direct register access model and software driver model can be used together in a single application, thus applying the most appropriate model as needed to any particular situation within the application. For example, the software driver model can be used to configure the peripherals (because this is not performance critical) and the direct register access model can be used to operate the peripheral (which may be more performance critical). Or, the software driver model can be used for peripherals that are not performance critical (such as a UART used for data logging) and the direct register access model can be used for performance critical peripherals.
In order to free up code space in the flash memory for user applications a part of the driver library has been stored in the on-chip ROM which allows the user to chose between calling certain drivers from either ROM or flash. Calling the ROM version of a driver function prevents the compiler from putting the function in flash and thus leaving more flash memory for applications.
Besides saving space in flash other benefits of using the ROM version of a driver library function are faster execution and reduced power consumption as flash is both slower and more power consuming than the ROM. A minor disadvantage of calling a ROM function is a small overhead in the function call as it does a table look-up to find the address of the ROM function. However, only driver library functions of a certain size have been selected to be stored in ROM which means that the ROM version of a function is always faster and less power consuming than its flash equivalent.
Because of the benefits of using the ROM version of a given driver a mechanism to select the ROM version as default has been implemented. This mechanism uses defines to effectively rename functions and function calls to distinguish between ROM and flash versions.
The mechanism works like this:
rom.h contains the list of ROM functions available in the device and each ROM function has a define that tells the compiler where to find the function in ROM (via a look-up table). All ROM functions have the prefix ROM_.static inline are defined (renamed) from FunctionName() to NOROM_FunctionName() thus all flash functions now have the prefix NOROM_ - except static inline functions which will keep the original name.ROM_ thus when a user includes the .h file in his .c file then all DriverLib calls are redefined to call the ROM function. The default redefinition to ROM functions can be avoided by defining DRIVERLIB_NOROM in the project. This will prevent the redefinition to ROM_ functions and keep the definition to NOROM_ functions and thus always use the flash version.static inline functions are redefined to NOROM_FunctionName in order to make sure that the functions in the DriverLib .c file are always redefined to have the prefix NOROM_ i.e. calling a NOROM_ function will always call the flash version.In summary: By default, the compiler will use DriverLib in ROM whenever possible and if the user wishes to avoid the ROM versions entirely (e.g. test and debugging) he can make a project-wide define called DRIVERLIB_NOROM which forces DriverLib to ignore the ROM functions. However, some functions from the flash API will always execute from ROM as they are not allowed to execute from flash (e.g. program and erase).
If a user wishes to avoid ROM versions of DriverLib by default but only use specific DriverLib functions from ROM this is possible:
DRIVERLIB_NOROM in the project to use flash versions as default.rom.h in the user .c file.ROM_ whenever a ROM function is wanted.If ROM functions are used as default then it is possible to use the flash version of a specific function:
NOROM_ whenever a flash function is wanted.NOROM_ explicitly to call the flash version of a DriverLib function (FunctionA) and that function makes a function call to another DriverLib function (FunctionB) then the internal function call (to FunctionB) will use the global selection; in this case the ROM version.When using the pre-compiled version of DriverLib then setting the define DRIVERLIB_NOROM in the project has no effect on the library itself. Thus all internal calls in the pre-compiled library to other DriverLib functions will always be to ROM version - if it exists.
Besides the functions available in the DriverLib a number of functions are also available in a ROM-only version. These functions are called HAPI functions (Hard API) and are generally used by various tools. Source code is not available for the HAPI functions but the functions are available for users to call. The list of HAPI functions available can be found in rom.h.
Invalid arguments and error conditions are handled in a non-traditional manner in DriverLib. Typically, a function would check its arguments to make sure that they are valid (if required; some may be unconditionally valid such as a 32-bit value used as the load value for a 32-bit timer). If an invalid argument is provided, an error code would be returned. The caller then has to check the return code from each invocation of the function to make sure that it succeeded.
This method results in a significant amount of argument-checking code in each function and return-code-checking code at each call site. For a self-contained application, this extra code becomes an unneeded overhead once the application is debugged. Having a means of removing it allows the final code to be smaller and therefore run faster and consume less power.
In this driver library, most functions do not return error status. Argument checking is done via a call to the ASSERT macro (provided in debug.h). This macro has the usual definition of an assert macro; it takes an expression that must be true. By making this macro empty, the argument checking is completely removed from the code thus avoiding the error checking overhead.
There are two definitions of the ASSERT macro provided in debug.h; one that is empty (used for normal/release builds) and one that evaluates the expression (used when the library is built for debugging). The debug version calls the __error__ function whenever the expression is not true, passing the file name and line number of the ASSERT macro invocation. The __error__ function is prototyped in debug.h and must be provided by the application because it is the application's responsibility to deal with error conditions.
To enable the ASSERT macro define the symbol DRIVERLIB_DEBUG within your project and/or compiler setup.
DRIVERLIB_DEBUG for the entire project might result in a significant increase in code size depending on the number of modules used in the project. Defining DRIVERLIB_DEBUG for specific files is possible if a project-wide define results in an unacceptable code size increase.By setting a breakpoint on the __error__ function, the debugger immediately stops whenever an error occurs anywhere in the application (something that would be very difficult to do with other error checking methods). When the debugger stops, the arguments to the __error__ function and the backtrace of the stack pinpoint the function that found an error, what it found to be a problem, and where it was called from. As an example:
Each argument is individually checked, so the line number of the failing ASSERT indicates the argument that is invalid. The debugger is able to display the values of the arguments (from the stack backtrace) as well as the caller of the function that had the argument error. This method allows the problem to be quickly identified at the cost of a small amount of code.
DriverLib includes a special function called trimDevice() which must always be called right after the ROM boot sequence in order to apply trim settings and certain customer configurations (from CCFG) to the device.
CC13/26xxWare also includes a customer configuration file (ccfg.c) which contains settings that are being applied mainly by ROM boot sequence, trimDevice() during startup, and radio SW. The configuration settings are stored in a specially allocated address range in flash referred to as "CCFG area". The user must edit the CCFG to fit the needs of the specific design and application.
Typically, a user application does not need to read the settings in CCFG; however, a few settings might be interesting for a user to read thus DriverLib provides an API that allows simple access to a subset of the CCFG settings (see the CCFGRead API). The remaining settings not covered by the DriverLib API can of course be read using the "Direct Register Access Model" described earlier. Although located in flash the CCFG settings are documented in the register descriptions as part of the CPU Domain Memory Map.
Texas Instruments provides a Real-Time Operating System (RTOS) for CC13xx called TI-RTOS which uses the DriverLib as the main interface to access the hardware registers thus minimizing the need for direct register accesses from TI-RTOS itself. The TI-RTOS package provides its own set of RTOS drivers that call DriverLib functions but RTOS drivers can be used only together with TI-RTOS and not stand-alone in a non-RTOS application.
When using TI-RTOS and the included RTOS drivers it is important that a user application does not "bypass" TI-RTOS drivers by calling DriverLib functions directly to configure any hardware that is controlled by TI-RTOS. Doing so can cause a conflict that may result in unexpected behavior by the RTOS.