66 #define GATT_CLIENT_CHAR_CFG_UPDATED_EVENT 0x00
75 #define GATT_PROP_BCAST 0x01
76 #define GATT_PROP_READ 0x02
77 #define GATT_PROP_WRITE_NO_RSP 0x04
78 #define GATT_PROP_WRITE 0x08
79 #define GATT_PROP_NOTIFY 0x10
80 #define GATT_PROP_INDICATE 0x20
81 #define GATT_PROP_AUTHEN 0x40
82 #define GATT_PROP_EXTENDED 0x80
90 #define GATT_EXT_PROP_RELIABLE_WRITE 0x0001
91 #define GATT_EXT_PROP_WRITABLE_AUX 0x0002
99 #define GATT_CLIENT_CFG_NOTIFY 0x0001
100 #define GATT_CLIENT_CFG_INDICATE 0x0002
108 #define GATT_SERV_CFG_BCAST 0x0001
112 #define GATT_CFG_NO_OPERATION 0x0000 // No operation
118 #define GATT_FORMAT_BOOL 0x01
119 #define GATT_FORMAT_2BIT 0x02
120 #define GATT_FORMAT_NIBBLE 0x03
121 #define GATT_FORMAT_UINT8 0x04
122 #define GATT_FORMAT_UINT12 0x05
123 #define GATT_FORMAT_UINT16 0x06
124 #define GATT_FORMAT_UINT24 0x07
125 #define GATT_FORMAT_UINT32 0x08
126 #define GATT_FORMAT_UINT48 0x09
127 #define GATT_FORMAT_UINT64 0x0a
128 #define GATT_FORMAT_UINT128 0x0b
129 #define GATT_FORMAT_SINT8 0x0c
130 #define GATT_FORMAT_SINT12 0x0d
131 #define GATT_FORMAT_SINT16 0x0e
132 #define GATT_FORMAT_SINT24 0x0f
133 #define GATT_FORMAT_SINT32 0x10
134 #define GATT_FORMAT_SINT48 0x11
135 #define GATT_FORMAT_SINT64 0x12
136 #define GATT_FORMAT_SINT128 0x13
137 #define GATT_FORMAT_FLOAT32 0x14
138 #define GATT_FORMAT_FLOAT64 0x15
139 #define GATT_FORMAT_SFLOAT 0x16
140 #define GATT_FORMAT_FLOAT 0x17
141 #define GATT_FORMAT_DUINT16 0x18
142 #define GATT_FORMAT_UTF8S 0x19
143 #define GATT_FORMAT_UTF16S 0x1a
144 #define GATT_FORMAT_STRUCT 0x1b
151 #define GATT_NS_NONE 0x00
152 #define GATT_NS_BT_SIG 0x01
153 #define GATT_NS_BT_DESC_UNKNOWN 0x0000
156 #define GATT_ALL_SERVICES 0xFFFFFFFF
160 #define GATT_SERVICE 0x00000001
163 #if defined ( TESTMODES )
165 #define GATT_TESTMODE_OFF 0 // Test mode off
166 #define GATT_TESTMODE_NO_RSP 1 // Ignore incoming request
167 #define GATT_TESTMODE_PREPARE_WRITE 2 // Forward Prepare Write Request right away
168 #define GATT_TESTMODE_MAX_MTU_SIZE 3 // Use Max ATT MTU size with Exchange MTU Rsp
169 #define GATT_TESTMODE_CORRUPT_PW_DATA 4 // Corrupt incoming Prepare Write Request data
176 #define GATT_PARAM_NUM_PREPARE_WRITES 0 // RW uint8
179 #define PTR_TYPE unsigned int *
185 #define GATT_LOCAL_READ 0xFF
186 #define GATT_LOCAL_WRITE 0xFE
200 #define GATT_NUM_ATTRS( attrs ) ( sizeof( attrs ) / sizeof( gattAttribute_t ) )
203 #define GATT_SERVICE_HANDLE( attrs ) ( (attrs)[0].handle )
206 #define GATT_INCLUDED_HANDLE( attrs, i ) ( *((uint16 *)((attrs)[(i)].pValue)) )
209 #define GATT_CCC_TBL( pValue ) ( (gattCharCfg_t *)(*((PTR_TYPE)(pValue))) )
251 uint8 *pValue, uint16 *pLen, uint16 offset,
252 uint16 maxLen, uint8 method );
286 uint8 *pValue, uint16 len, uint16 offset,
424 uint16 numAttrs, uint8 encKeySize,
455 uint16 numAttrs, uint8 *pValue );
596 uint8 *pValue, uint16 len, uint16 offset,
619 uint16 numAttrs, uint8 taskId,
665 uint16 service, uint8 *pValue, uint16 *pLen,
666 uint16 offset, uint16 maxLen, uint8 method );
682 uint8 *pValue, uint16 len, uint16 offset,
699 uint16 pLen, uint16 offset );
732 extern void GATTServApp_Init( uint8 taskId );
745 extern uint16 GATTServApp_ProcessEvent( uint8 taskId, uint16 events );
809 extern bStatus_t gattServApp_buildReadByTypeRsp( uint16 connHandle, uint8 *pAttrValue, uint16 attrLen, uint16 attrHandle );
820 extern prepareWrites_t *gattServApp_FindPrepareWriteQ( uint16 connHandle );
uint16 GATTServApp_GetParamValue(void)
Get a GATT Server Application Parameter value.
This API allows the software components in the Z-Stack to be written independently of the specifics o...
uint16 connHandle
Connection message was received on.
Definition: gattservapp.h:342
GATT Server App event header format.
Definition: gattservapp.h:339
void GATTServApp_SetParamValue(uint16 value)
Set a GATT Server Application Parameter value. Use this function to change the default GATT parameter...
gattAttribute_t * GATTServApp_FindAttr(gattAttribute_t *pAttrTbl, uint16 numAttrs, uint8 *pValue)
Find the attribute record within a service attribute table for a given attribute value pointer...
pfnGATTAuthorizeAttrCB_t pfnAuthorizeAttrCB
Authorization callback function pointer.
Definition: gattservapp.h:335
Service callbacks list item.
Definition: gattservapp.h:377
void GATTServApp_SendCCCUpdatedEvent(uint16 connHandle, uint16 attrHandle, uint16 value)
Build and send the GATT_CLIENT_CHAR_CFG_UPDATED_EVENT to the application.
Structure to keep Prepare Write Requests for each Client.
Definition: gattservapp.h:363
bStatus_t GATTServApp_GetParameter(uint8 param, void *pValue)
Get a GATT Server parameter.
pfnGATTWriteAttrCB_t pfnWriteAttrCB
Write callback function pointer.
Definition: gattservapp.h:334
prepareWrites_t * prepareWritesTbl
Server Prepare Write table (one entry per each physical link)
GATT Structure to keep CBs information for each service being registered.
Definition: gattservapp.h:370
uint8 value
Characteristic configuration value for this client.
Definition: gattservapp.h:322
bStatus_t GATTServApp_AddService(uint32 services)
Add function for the GATT Service.
bStatus_t(* pfnGATTReadAttrCB_t)(uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint16 *pLen, uint16 offset, uint16 maxLen, uint8 method)
Callback function prototype to read an attribute value.
Definition: gattservapp.h:250
pfnGATTReadAttrCB_t pfnReadAttrCB
Read callback function pointer.
Definition: gattservapp.h:333
bStatus_t(* pfnGATTWriteAttrCB_t)(uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint16 len, uint16 offset, uint8 method)
Callback function prototype to write an attribute value.
Definition: gattservapp.h:285
bStatus_t GATTServApp_ReadRsp(uint16 connHandle, uint8 *pValue, uint16 pLen, uint16 offset)
If a service returns blePending to the read attribute call back invoked from GATTServApp, the service can later respond to with the value to be read using this API.
uint8 GATTServApp_WriteAttr(uint16 connHandle, uint16 handle, uint8 *pValue, uint16 len, uint16 offset, uint8 method)
Write attribute data.
Structure for Client Characteristic Configuration.
Definition: gattservapp.h:319
osal_event_hdr_t hdr
GATT_SERV_MSG_EVENT and status.
Definition: gattservapp.h:341
uint16 connHandle
Client connection handle.
Definition: gattservapp.h:321
bStatus_t GATTServApp_ProcessCharCfg(gattCharCfg_t *charCfgTbl, uint8 *pValue, uint8 authenticated, gattAttribute_t *attrTbl, uint16 numAttrs, uint8 taskId, pfnGATTReadAttrCB_t pfnReadAttrCB)
Process Client Characteristic Configuration change.
uint16 GATTServApp_ReadCharCfg(uint16 connHandle, gattCharCfg_t *charCfgTbl)
Read the client characteristic configuration for a given client.
void GATTServApp_RegisterForMsg(uint8 taskID)
Register your task ID to receive event messages from the GATT Server Application. ...
void GATTServApp_InitCharCfg(uint16 connHandle, gattCharCfg_t *charCfgTbl)
Initialize the client characteristic configuration table.
uint16 value
attribute new value
Definition: gattservapp.h:358
uint16 connHandle
Connection message was received on.
Definition: gattservapp.h:355
Type definitions and macros for BLE stack.
bStatus_t GATTServApp_SetParameter(uint8 param, uint8 len, void *pValue)
Set a GATT Server parameter.
bStatus_t GATTServApp_SendServiceChangedInd(uint16 connHandle, uint8 taskId)
Send out a Service Changed Indication.
bStatus_t GATTServApp_DelService(uint32 services)
Delete function for the GATT Service.
uint16 attrHandle
attribute handle
Definition: gattservapp.h:357
serviceCBsList_t * serviceCBsList
Callbacks for services.
OSAL Event Header.
Definition: osal.h:110
GATT_CLIENT_CHAR_CFG_UPDATED_EVENT message format.
Definition: gattservapp.h:352
struct _serviceCBsList serviceCBsList_t
Service callbacks list item.
GATT GATT_MSG_EVENT message format.
Definition: gatt.h:231
uint8 method
GATT type of command. Ref: GATT Server Message IDs.
Definition: gattservapp.h:343
bStatus_t GATTServApp_RegisterService(gattAttribute_t *pAttrs, uint16 numAttrs, uint8 encKeySize, CONST gattServiceCBs_t *pServiceCBs)
Register a service's attribute list and callback functions with the GATT Server Application.
bStatus_t GATTServApp_ProcessCCCWriteReq(uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint16 len, uint16 offset, uint16 validCfg)
Process the client characteristic configuration write request for a given client. ...
osal_event_hdr_t hdr
GATT_SERV_MSG_EVENT and status.
Definition: gattservapp.h:354
GATT Attribute format.
Definition: gatt.h:260
Status_t bStatus_t
BLE Generic Status return.
Definition: bcomdef.h:243
bStatus_t(* pfnGATTAuthorizeAttrCB_t)(uint16 connHandle, gattAttribute_t *pAttr, uint8 opcode)
Callback function prototype to authorize a Read or Write operation on a given attribute.
Definition: gattservapp.h:299
Prepare Write Request format.
Definition: att.h:553
uint8 method
GATT_CLIENT_CHAR_CFG_UPDATED_EVENT.
Definition: gattservapp.h:356
bStatus_t GATTServApp_UpdateCharCfg(uint16 connHandle, uint16 attrHandle, uint16 value)
Update the Client Characteristic Configuration for a given Client.
uint8 GATTServApp_WriteCharCfg(uint16 connHandle, gattCharCfg_t *charCfgTbl, uint16 value)
Write the client characteristic configuration for a given client.
GATT Structure for service callback functions.
Definition: gattservapp.h:331
Execute Write Request format.
Definition: att.h:579
bStatus_t GATTServApp_DeregisterService(uint16 handle, gattAttribute_t **p2pAttrs)
Deregister a service's attribute list and callback functions from the GATT Server Application...
uint8 GATTServApp_ReadAttr(uint16 connHandle, gattAttribute_t *pAttr, uint16 service, uint8 *pValue, uint16 *pLen, uint16 offset, uint16 maxLen, uint8 method)
Read an attribute. If the format of the attribute value is unknown to GATT Server, use the callback function provided by the Service.